This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCO来设计时钟,精度可靠吗?



要设计一个时钟,用片内的DCO,这样可行吗?或者我用时钟芯片来,这样精确度会更高。

  • 430内部DCO精度和VCC和温度相关,全温度全电压范围(-40--+85°)(1.8V--3.6V)情况下误差±5%。常温下约1%。

    所以精度要求不高的情况下,可以使用430内部DCO

    如果需要更高精度,可以用外部晶体作为时钟源。比如20ppm的crystal。