This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本公司一种仪表原使用C8051F020单片机(100脚,25m,64k,2串口,8路12位AD),欲改为MSP430系列单片机重新设计,突出低功耗功能,以下几种可能方案哪个好些?(以性能、扩展、资源、价格顺序筛选)
F149
F249
F2618
F5438
建议采用F5xxx系列的产品,例如F5438,这个系列可以达到25Mhz, 也是功耗最低的系列,
如果64K flash 足够的,您可以采用 MSP430F5324: