各位老师:大家好!
我在进行MSP430F5529的BSL代码修改时遇到了一些问题。在解锁BSL会默认进行除BSL代码段及information段的所有代码的擦除,现在修改BSL源代码,在输入错误BSL密码后,不希望全部擦除main memory存储区的部分代码,采用按段擦除,在usb模式下可行,在uart模式下却必须进行整体擦除才可行。是否usb和uart模式下在输入错误密码擦除时存在其他问题?还有,在函数中block_erase==1时进行块擦除也无法实现块擦除,是否按地址擦除代码存在问题?谢谢!!!
代码如下:芯片选型5529
//0--3 usb_ram;4--19 ram;20--147 main memory bank a and b; 148--211 bank c; 212--275 bank d;
long addre=0x1c00;
for(int mm=0;mm<148;mm++) //276
{
BSL430_eraseLocation(0, addre);//usb ram ~~bank b
addre=addre+512;
}
char BSL430_eraseLocation(char block_erase, unsigned long addr)
{
char exceptions;
if (LockedStatus == UNLOCKED || 0 == earseflash)
{
exceptions = SUCCESSFUL_OPERATION;
#ifdef RAM_BASED_BSL
while (FCTL3 & BUSY) ;
#endif
FCTL3 = FwRamKey; // Clear Lock bit
if(0==block_erase)
FCTL1 = FwRamKey + ERASE; // Set Erase bit
else
FCTL1 = FwRamKey + MERAS; // Set Erase bit
__data20_write_char(addr, 0); // Dummy write to erase Flash seg
#ifdef RAM_BASED_BSL
while (FCTL3 & BUSY) ;
#endif
FCTL3 = FwRamKey + LOCK; // Set LOCK bit
}
else
{
exceptions = BSL_LOCKED;
}
return exceptions;
}