This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM TI例程的疑问

Other Parts Discussed in Thread: MSP430F149

//
//  // 
//
//               MSP430F149
//            -----------------
//        /||              XIN|-
//         | |                 | HF XTAL (455k - 8MHz)
//         --|RST          XOUT|-
//           |                 |
//           |         P4.1/TB1|--> CCR1 - 75% PWM
//           |         P4.2/TB2|--> CCR2 - 25% PWM
//
//  M. Buccini
//  Texas Instruments Inc.
//  Feb 2005
//  Built with IAR Embedded Workbench Version: 3.21A
//******************************************************************************
#include  <msp430x14x.h>
void main(void)
{
  volatile unsigned int i;
  WDTCTL = WDTPW +WDTHOLD;                  // Stop WDT
//系统时钟初始化
  BCSCTL1 |= XTS;                           // ACLK= LFXT1 = HF XTAL
  do
  {
  IFG1 &= ~OFIFG;                           // Clear OSCFault flag
  for (i = 0xFF; i > 0; i--);               // Time for flag to set
  }
  while ((IFG1 & OFIFG));                   // OSCFault flag still set?
  BCSCTL2 |= SELM_3;                        // MCLK= LFXT1 (safe)
//io口初始化
  P4DIR |= 0x06;                            // P4.1 and P4.2 output
  P4SEL |= 0x06;                            // P4.2 and P4.2 TB1/2 otions
//定时器B的配置
  TBCCR0 = 128;                             // PWM Period/2
  TBCCTL1 = OUTMOD_6;                       // CCR1 toggle/set
  TBCCR1 = 32;                              // CCR1 PWM duty cycle
  TBCCTL2 = OUTMOD_6;                       // CCR2 toggle/set
  TBCCR2 = 96;                              // CCR2 PWM duty cycle
  TBCTL = TBSSEL_1 + MC_3;                  // ACLK, up-down mode
  _BIS_SR(CPUOFF);                          // Enter LPM0
}

我不明白“toggle/set”是什么意思?
还有do while这个循环体可以不要吗?没有打开XT2OFF应该不用起振吧?
  • Hi 楼主,

       建议你先查看一下我们MSP430F149的技术手册,里面针对timer模块有相应的各种模式。这里的例子选择的是mode6, toggle/set是指翻转,跳转的意思。简单点说就是计数器记到CCR1的值时电平跳到高电平,然后一直记下去,到TBCCR0(128)是在转为低电平,然后在重新加到CCR1是跳到高电平。这样就可以实现占空比为75%的方波,同理,TBCCR2实现的是占空比为25%的波形。

       do while这个循环体主要是用来判断外部晶振是否稳定的一个操作。如果你选择使用芯片内部的晶振的话,可以不需要这个循环体,但是如果要用到外部高频晶振的话,这个还是需要保留的。

    谢谢

    ken