Other Parts Discussed in Thread: MSP430F149
//
// //
//
// MSP430F149
// -----------------
// /|| XIN|-
// | | | HF XTAL (455k - 8MHz)
// --|RST XOUT|-
// | |
// | P4.1/TB1|--> CCR1 - 75% PWM
// | P4.2/TB2|--> CCR2 - 25% PWM
//
// M. Buccini
// Texas Instruments Inc.
// Feb 2005
// Built with IAR Embedded Workbench Version: 3.21A
//******************************************************************************
#include <msp430x14x.h>
void main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW +WDTHOLD; // Stop WDT
//系统时钟初始化
BCSCTL1 |= XTS; // ACLK= LFXT1 = HF XTAL
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while ((IFG1 & OFIFG)); // OSCFault flag still set?
BCSCTL2 |= SELM_3; // MCLK= LFXT1 (safe)
//io口初始化
P4DIR |= 0x06; // P4.1 and P4.2 output
P4SEL |= 0x06; // P4.2 and P4.2 TB1/2 otions
//定时器B的配置
TBCCR0 = 128; // PWM Period/2
TBCCTL1 = OUTMOD_6; // CCR1 toggle/set
TBCCR1 = 32; // CCR1 PWM duty cycle
TBCCTL2 = OUTMOD_6; // CCR2 toggle/set
TBCCR2 = 96; // CCR2 PWM duty cycle
TBCTL = TBSSEL_1 + MC_3; // ACLK, up-down mode
_BIS_SR(CPUOFF); // Enter LPM0
}
我不明白“toggle/set”是什么意思?
还有do while这个循环体可以不要吗?没有打开XT2OFF应该不用起振吧?