This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6726最小系统问题

Other Parts Discussed in Thread: MSP430F6726

将MSP430F6726焊在QFP转接板后,通过杜邦线连在面包板上面,做成一个最小系统(主要是将AVCC、DVCC连在VCC上,AVSS、DVSS、AUXVCC1、AUXVCC2连在VSS上,VDSYS与DVSYS、AUXVCC3连接,VCORE接470nF电容到地),引出JTAG通信引脚提示找不到器件,经过排查,发现VCORE电压为2.8V左右。换一个芯片,这次接好其他电路后不接JTAG引脚,直接测量VCORE电压,发现仍为2.8V左右。VCORE是1.8V左右才正常是吗?那出现2.8V的情况可能是什么原因呢?

  • MSP430F67XX layout checklist

    1, VCORE 引脚外接滤波电容必须为470nF。

    2, LCDCAP/R33 引脚如果没有使用,必须接到DVSS。

    3, VDSYS、DVSYS引脚必须连接在一起。

    4, AVCC,DVCC使用同一个电压源供电。在上电和工作的时候,AVCC 和 DVCC电压压差不应超过0.3V。

  • 5, DVCC, AVCC, AUX1, AUX2 pin 推荐电源退耦合/滤波电容为4.7uF。

    6, VDSYS、VASYS推荐推荐电源退耦合/滤波电容为4.7uF。

    7, AUX3推荐推荐推荐电源退耦合/滤波电容为0.47uF。 8, VREF 引脚滤波电容尽可能就近引脚放置。

    9, EMC:SEG,COM引脚内阻为700~800ohm, SEG片外最大9Kohm,COM片外最大300Ohm。