例如一个长度为64字节的一维数组,想将其写入在MSP430的0xFA00开始的位置,即编译后这个数组的起始位置为0xFA00,C程序中如何处理呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
例如一个长度为64字节的一维数组,想将其写入在MSP430的0xFA00开始的位置,即编译后这个数组的起始位置为0xFA00,C程序中如何处理呢?
刚查了MSP430 C compiler User Guide,没查到@的这个用法,是在这片文档里提及的嘛?
Charles,
在《Code Composer Studio™ v4.2 User's Guide for MSP430™ User's Guide》www.ti.com/.../slau157s.pdf 29页有这种用法。
以下为相应段落:
”
The scheme implemented in the IAR compiler using either the @ operator or the #pragma location directive is not supported with the CCS compiler:
/* IAR C Code */
__no_init char alpha @ 0x0200; /* Place ‘alpha' at address 0x200 */
#pragma location = 0x0202
const int beta;
“
const char alpha @ 0x0200;也是可以的。
见过Jason用过@这种用法,学习来的。但是在CCS中不支持。
QQ群内有人提出这种处理方式,添加一个汇编文件定义:
新建汇编文件.ASM
文件内容
ORG 0FA00H
数据
END
汇编文件添加到工程中,不用调用的
你好,请问ccs中应该怎样定义呢?将数组指定到flash的固定地址