各位自身FAE和大神
请问:
TSS 721 A芯片采用远程供电时,芯片的VDD最多能提供多大的电流?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The maximum current provided by the TSS721A depends the design of the slave device. In general, a slave device can draw 1 unit load from the MBUS, which is 1.5mA max. The TSS721A can be configured to draw 2 unit load (<3mA) from the MBUS. And the TSS721A consumes 650uA from the bus. So the avaliable current output from the VDD is Ibus - Icc.