This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
//****************************************************************************** // MSP-FET430P140 Demo - Basic Clock, Implement Auto RSEL SW FLL // // Description: Set DCO clock to (Delta)*(4096) using software FLL. DCO clock // is output on P5.5 as SMCLK. DCO clock, which is the selected SMCLK source // for timer_A is integrated over LFXT1/8 (4096) until SMCLK is is equal // to Delta. CCR2 captures ACLK. To use Set_DCO Timer_A must be // operating in continous mode. Watch crystal for ACLK is required for // this example. Delta must be kept in a range that allows possible // DCO speeds. Minimum Delta must ensure that Set_DCO loop // can complete within capture interval. Maximum delta can be calculated be // f(DCOx7) / 4096. f(DCOx7) can be found in device specific datasheet. // ACLK = LFXT1/8 = 32768/8, MCLK = SMCLK = target DCO // //* External watch crystal installed on XIN XOUT is required for ACLK *// // // MSP430F149 // --------------- // /|\| XIN|- // | | | 32kHz // --|RST XOUT|- // | | // | P5.5|--> SMLCK = target DCO // | P5.6|--> ALCK = 4096 // // // M. Buccini // Texas Instruments Inc. // Feb 2005 // Built with IAR Embedded Workbench Version: 3.21A //****************************************************************************** #include <msp430x14x.h> void Set_DCO (void); void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT P5DIR |= 0x60; // P5.5,6 output P5SEL |= 0x60; // P5.5,6 SMCLK, ACLK output Set_DCO(); // Set DCO while (1); } //------------------------------------------------------------------------------ void Set_DCO (void) // Set DCO to selected frequency //------------------------------------------------------------------------------ { //#define DELTA 900 // target DCO = DELTA*(4096) = 3686400 #define DELTA 256 // target DCO = DELTA*(4096) = 1048576 //#define DELTA 70 // target DCO = DELTA*(4096) = 286720 unsigned int Compare, Oldcapture = 0; BCSCTL1 |= DIVA_3; // ACLK= LFXT1CLK/8 CCTL2 = CM_1 + CCIS_1 + CAP; // CAP, ACLK TACTL = TASSEL_2 + MC_2 + TACLR; // SMCLK, cont-mode, clear while (1) { while (!(CCIFG & CCTL2)); // Wait until capture occured CCTL2 &= ~CCIFG; // Capture occured, clear flag Compare = CCR2; // Get current captured SMCLK Compare = Compare - Oldcapture; // SMCLK difference Oldcapture = CCR2; // Save current captured SMCLK if (DELTA == Compare) break; // If equal, leave "while(1)" else if (DELTA < Compare) // DCO is too fast, slow it down { DCOCTL--; if (DCOCTL == 0xFF) { if (!(BCSCTL1 == (XT2OFF + DIVA_3))) BCSCTL1--; // Did DCO roll under?, Sel lower RSEL } } else { DCOCTL++; if (DCOCTL == 0x00) { if (!(BCSCTL1 == (XT2OFF + DIVA_3 + 0x07))) BCSCTL1++; // Did DCO roll over? Sel higher RSEL } } } CCTL2 = 0; // Stop CCR2 TACTL = 0; // Stop Timer_A }
1.为什么使用Timer_A2的捕获模式、CCI2B捕获输入,而不设置P4.2引脚为第二功能、输入状态呢?
2. “if (DCOCTL == 0xFF)”和“if (DCOCTL == 0x00)”里面的语句不懂表达什么意思?
楼主,
我觉得应该这么理解者两个问题:
1.可以参考datasheet的timer_A3的介绍。在一个表里面有写到CCI2B被内部连接到了ACLK上了,而不是用的P4.2脚;
2.因为是根据捕捉的值来调整DCOx和RSELx来调整DCO的,DCOx是粗调,RSELx是细调。当粗调调到顶(if (DCOCTL == 0xFF)”)或者调到底(if (DCOCTL == 0x00)”)的时候,就需要调整一下RSELx再试试了。
明白,请问同步捕获与异步捕获的区别是?step by step 说:楼主,
我觉得应该这么理解者两个问题:
1.可以参考datasheet的timer_A3的介绍。在一个表里面有写到CCI2B被内部连接到了ACLK上了,而不是用的P4.2脚;
2.因为是根据捕捉的值来调整DCOx和RSELx来调整DCO的,DCOx是粗调,RSELx是细调。当粗调调到顶(if (DCOCTL == 0xFF)”)或者调到底(if (DCOCTL == 0x00)”)的时候,就需要调整一下RSELx再试试了。
楼主,
同步捕获的捕获中断产生的时刻是在捕获产生后紧接着的clk的下降沿;而异步捕获中断发生在捕获事件发生的时候。推荐使用同步捕获。
还是有点疑惑,SMCLK和ACLK都设置为在管脚输出了,那timer从哪里捕获的呢?CCI2B是timer的输入,又是比较器的输出,但是比较器好像没有设置输入啊?请问timer是如何捕获ACLK的呢?