This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

利用430F169控制pwm输出脉冲的个数



#include <msp430x16x.h>
#define CPU_F ((double)8000000)
#define delay_us(x)__delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x)__delay_cycles((long)(CPU_F*(double)x/1000.0))
void main()
{
WDTCTL = WDTPW + WDTHOLD; //停止看门狗WDT,不使用内部看门狗定时器。
P1DIR |= 0x01; //设置P1.0口方向为输出。
CCTL0 = CCIE; //设置捕获/比较控制寄存器中CCIE位为1,CCR0捕获/比较功能中断为允许。
TACCR0 = 110; //捕获/比较控制寄存器CCR0初值为110。
TACTL = TASSEL_1 + MC_2; //设置定时器A控制寄存器TACTL,使时钟源选择为CLK辅助时钟。
_BIS_SR(LPM0_bits + GIE); //进入低功耗模式LPM0和开中断
}

//定时器A 中断服务程序区

#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A (void)
{
P1OUT ^= 0x01; //P1.0取反输出
TACCR0 += 110; //重新载入CCR0捕获/比较数据寄存器数据
//delay_ms(1000);
}    

  如何控制它输出3200个脉冲????????