This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD16_A的输入电压范围

Other Parts Discussed in Thread: MSP430F478

您好,我想问一下,对于MSP430F478的的SD16_A,外部参考Vref可否直接接到Vcc(3.3V),如果可以的话,它的可检测的输入电压信号范围是多少?0~3.3V还是0~1.65V呢?如果我要检测的信号是5V,那么需要如何处理呢?谢谢~~

  • 楼主,

            外部参考值应该为1.25v,不能接到vcc。输入电压范围在+-vref/(2*gain)。如果是5v的检测信号,可以做分压处理

  • 谢谢~~还有两个问题需要您的热心帮助。

    第一个问题:芯片上的Vref管脚只能最大接到1.25V对吗?如果我的信号是单端输入的呢?量程是0~1.25还是0~0.625呢?

    第二个问题:SD16_A里面有PGA模块,如果我要检测的电压是0~5V,需要前置分压电路,分压的输出可以直接接入SD16_A的输入吗?或者需要再连接一个电压跟随器来保证电压不会有损耗吗?

    非常感谢~~