This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5418换成5418A后时钟问题



我以前用的是5418,现在用5418A,晶振初始化部分没变,为什么记录24小时时钟慢慢变快了?

  • 这个可能的原因很多了。给您一个文档,按照文档上说的改一下看看。

    www.ti.com/.../slaa419b.pdf

  • 我已经看过了,下面是我设置晶振的程序,麻烦帮我看一下是不是PMM部分有问题?

    void InitialCPU(void)

    {

    /********************设置晶振****************/

     WDTCTL = WDTPW + WDTHOLD;              //关看门狗,应放置在第一条可执行语句处

    P7SEL |= 0x03;                            // Analog function for XT1 Pins  

     UCSCTL6 &= ~XT1DRIVE_3;                   // Lowest drive strength

     UCSCTL6 |= XCAP_3 ;                       // Internal load cap    

     UCSCTL4  |= SELA__XT1CLK;  

     while ( (SFRIFG1 &OFIFG))

     {    

       UCSCTL7 &= ~(XT1LFOFFG + DCOFFG);

       SFRIFG1 &= ~OFIFG;

     }  

     UCSCTL0 = 0x00;                           // Set lowest possible DCOx, MODx

     UCSCTL1 = DCORSEL_7;                      // Select range for 20MHz operation

     PMMCTL0 = 0xA500 + PMMCOREV_3;              // Set VCore=1.9V

     SVSMLCTL = SVMLE + (PMMCOREV_3 * SVSMLRRL0);// Set SVM new Level ,  

     while ((PMMIFG & SVSMLDLYIFG) == 0);   // Wait till SVM is settled (Delay)

     PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);     // Clear already set flags

     if ((PMMIFG & SVMLIFG))

       while ((PMMIFG & SVMLVLRIFG) == 0);  // Wait till level is reached

     PMMCTL0_H = 0x00;                      // Lock PMM module registers

     UCSCTL2 =449;                            

     UCSCTL4 = SELS_3 + SELM_3;                // Set MCLK = SMCLK = DCOCLK    

  • 楼主还是把现象描述的再具体一点吧,什么叫做“慢慢变快了”?有量化的数据嘛?

  • 我连续采集数据,24小时后会提示记录结束,用5418A的后还没到24小时就提示了。而且一次和一次的时间还不定。数据够着呢~~~

  • 具体的数据?具体是差多少时间啊?