初学msp430 ,对其时钟配置不是很清楚。帮忙分析下这个代码
P5SEL |= 0x0C;
// Use the REFO oscillator as the FLL reference, and also for ACLK
UCSCTL3 = (UCSCTL3 & ~(SELREF_7)) | (SELREF__REFOCLK);
UCSCTL4 = (UCSCTL4 & ~(SELA_7)) | (SELA__XT2CLK);
// Start the FLL, which will drive MCLK (not the crystal)
Init_FLL(USB_MCLK_FREQ/1000, USB_MCLK_FREQ/32768);
我的外部时钟是24Mhz晶振。请问这个设置后我的ACLK,MCLK SMClK 分别是多少?基于这个配置下。我想用115200波特率的串口,那串口如何配置?
谢谢