请问定时器A,B之类的有些什么区别?能不能汇总列表对比一下?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Fuchong,
这个表没有,不过在User's Guide中有一些区别:
16.1.1 Similarities and Differences From Timer_A
Timer_B is identical to Timer_A with the following exceptions:
• The length of Timer_B is programmable to be 8, 10, 12, or 16 bits.
• Timer_B TBxCCRn registers are double-buffered and can be grouped.
• All Timer_B outputs can be put into a high-impedance state.
• The SCCI bit function is not implemented in Timer_B.
17.1.1 Differences From Timer_B
Timer_D is identical to Timer_B with the following exceptions:
• Timer_D supports high-resolution mode.
• Timer_D supports the combination of two adjacent TDCCRx registers in one capture/compare channel.
• Timer_D supports the dual capture event mode.
• Timer_D supports external fault input, external clear input, and signal. See the TEC chapter for
detailed information.
• Timer_D can synchronize with a second timer instance when available. See the TEC chapter for
detailed information