This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529 BoadLoader 自定义串口升级问题



BoadLoader:

升级程序空间:0XF000-0XFF7F

中断向量地址:0XFF80-0XFFFF

用户程序:

程序空间:0x4400-0xf000

中断向量地址:0xEF80-0XEFFF

本程序是共用同一个串口,上电时,串口用于升级代码,升级完成以后用于用户程序进行数据接收,使用变量UpdateOk进行区分,但现在问题是:升级完用户程序以后,用户程序里面的TimerA进中断出中断均没有问题,但是复用的串口有问题:

#pragma vector=USCI_A1_VECTOR

__interrupt void USCI_A1_ISR(void)

{

  if(UpdateOk==0)        //升级使用

  {

unsigned char temp;

switch(__even_in_range(UCA1IV,4))

{

case 0:break; // Vector 0 - no interrupt

case 2: // Vector 2 - RXIFG

while (!(UCA1IFG&UCTXIFG)); // USCI_A0 TX buffer ready?

Cmd=UCA1RXBUF;

CommandHandle();                      //这个程序是升级代码用的,只要他存在,在进行用户程序接收数据时,就出问题,出串口中断的时候,出栈错误,进入到boadloader里面的子函数(某一个固定的地址),进而程序跑飞,因此肯定是压栈出问题直接导致出栈出问题

break;

case 4:break; // Vector 4 - TXIFG

default: break;

}

  }else if(UpdateOk==1)     //用户程序接收数据用

  {

    asm("BR &0xEFDC");    //跳转到应用程序的串口中断向量

  }

}

程序框架:

void main(void)

{

/*** Basic Setting ***/

WDTCTL = WDTPW + WDTHOLD; // Stop WDT

    UpdateOk=0;  //升级变量

/*** Regular Init ***/

IOS_Init(); // IO口初始化

SCI_Init(); // 串口初始化

/*** Prepare Start ***/

EnableInterrupt;

delay(5);

SCI_TxStr((unsigned char *)Item1); // Send Item1 BootInformation

 

/*** Main Loop ***/等到2秒钟检测是否有串口数据的到来,如果有就进行升级,如果没有就asm("BR &0xEFFE");跳转到用户程序里的复位向量,进而执行应用程序

while( Waiting<30 )

{

P1OUT=0x01; // LED blink

delay(50);

P1OUT=0x02; // LED blink

delay(50);

if(FlxSts==UnBoot) // QuitTime Test

Waiting++;

if(FlxSts==QuitBoot) // Quit Directly

Waiting=100;

}

SCI_TxStr((unsigned char *)Item6); // Quit Bootloader

SCI_Deinit();

    UpdateOk=1;// Deinit SCI

    asm("BR &0xEFFE");

}

#pragma vector=TIMER0_A0_VECTOR

__interrupt void TIMER0_A0_ISR(void)

{

//  P1OUT ^= BIT3;                            // Toggle P1.0

    asm("BR &0xEFEA");                   //跳转到用户程序的定时器中断向量,这个工作完全正常

}

 

用户程序:

void main(void)

{

  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT

  P1DIR |= BIT3;                            // P1.0 output

  TA0CCTL0 = CCIE;                          // CCR0 interrupt enabled

  TA0CCR0 = 50000;

  TA0CTL = TASSEL_2 + MC_1 + TACLR;         // SMCLK, upmode, clear TAR

 

    P4SEL = BIT5+BIT4;                        // P3.4,5 = USCI_A0 TXD/RXD

  UCA1CTL1 |= UCSWRST;                      // **Put state machine in reset**

  UCA1CTL1 |= UCSSEL_2;                     // SMCLK

  UCA1BR0 = 6;                              // 1MHz 9600 (see User's Guide)

  UCA1BR1 = 0;                              // 1MHz 9600

  UCA1MCTL = UCBRS_0 + UCBRF_13 + UCOS16;   // Modln UCBRSx=0, UCBRFx=0,

                                            // over sampling

  UCA1CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**

  UCA1IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt

  

  

  __bis_SR_register(LPM0_bits + GIE);       // Enter LPM0, enable interrupts

  __no_operation();                         // For debugger

}

 

// Timer0 A0 interrupt service routine

#pragma vector=TIMER0_A0_VECTOR

__interrupt void TIMER0_A0_ISR(void)

{

  P1OUT ^= BIT3;                            // Toggle P1.0

}

#pragma vector=USCI_A1_VECTOR

__interrupt void USCI_A1_ISR(void)

{

  switch(__even_in_range(UCA1IV,4))

  {

  case 0:break;                             // Vector 0 - no interrupt

  case 2:                                   // Vector 2 - RXIFG

    while (!(UCA1IFG&UCTXIFG));             // USCI_A0 TX buffer ready?

    UCA1TXBUF = UCA1RXBUF;                  // TX -> RXed character

    break;

  case 4:break;                             // Vector 4 - TXIFG

  default: break;

  }

}