msp430-exp430f5529lp仿真时遇到如下错误
Error initializing emulator:
A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps).
DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
请问我应该如何处理?
需不需要换版本?
我电脑为win7 64bit ,ccs v6.0
仿真器为f5529launchpad上自带的ez-fet lite,仿真器芯片为msp430f5528
背面有一个白色的贴纸:3971418002104
我电脑昨天晚上刚重装了一次系统,环境为vc2005,vc2008,vc2010,以及这些东西的64位版本
java 是最新的版本,仿真器,uart,5529自带空间均能够识别
板子上的跳线帽连了SBW RST,SBW TST,TXD,RXD ,3V3,5V,GND
RTS和CTS没连