This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用MSP430F5529ADC12模块出现的问题

Other Parts Discussed in Thread: MSP430F5529

我利用网络资源和LAB1写了如下程序,结果出现这样的问题error #10056: symbol "timeoutCounter" redefined: first defined in "./lab1.obj";

error #10056: symbol "__TI_int54" redefined: first defined in "./lab1.obj";

"../lnk_msp430f5529.cmd", line 180: error #10099-D: program will not fit into

error #10010: errors encountered during linking; "LAB1.out" not built

多方查询没有什么结果-。-,程序如下

lab1:

#include <stdint.h>
#include "msp430.h"
#include "HAL_Buttons.h"
#include "HAL_Board.h"
#include "HAL_Dogs102x6.h"
#include "HAL_Menu.h"
#include "HAL_Wheel.h"
#include "lab1.h"


// This image has been created by ImageDog using 'small_sunglasses.png'
static const uint8_t sunglasses[] =
{
0x30, // Image width in pixels
0x06, // Image height in rows (1 row = 8 pixels)
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x01, 0x01, 0x03, 0x03, 0x07, 0x03, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0x03, 0x06, 0x1e, 0x1f, 0x3f, 0x7f,
0x7f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x3f, 0x1f, 0x03, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01,
0x01, 0x03, 0x03, 0x0f, 0x1e, 0x1c, 0x38, 0x30, 0x70, 0xf8, 0xfc, 0x0e, 0x07, 0xf3, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xfe, 0xfc, 0xf8, 0xf0, 0xc0, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0x03, 0x07, 0x0e, 0x1c, 0x3f, 0x7f, 0x7f, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x3f, 0x1f, 0x01, 0x00, 0x00, 0x00, 0x00, 0x80, 0x80, 0xc0,
0xc0, 0xc0, 0xc0, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x20, 0xf0, 0xf8, 0xf8, 0x3c, 0x0e, 0x07, 0xf7, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xfe, 0xfc, 0xf8, 0xf0, 0xe0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x80, 0x80, 0x80, 0x80, 0x80,
0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};
// This image has been created by ImageDog using 'lightbulb_outline_inverted_mini.png'
static const uint8_t lightbulb[] =
{
0x20, // Image width in pixels
0x06, // Image height in rows (1 row = 8 pixels)
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0x03, 0x06, 0x0c, 0x18, 0x10, 0x10, 0x10, 0x30, 0x00,
0x00, 0x00, 0x30, 0x11, 0x11, 0x11, 0x18, 0x0c, 0x04, 0x06, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x04, 0x7c, 0xc0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x40, 0xe0, 0x30, 0x9d, 0xcf, 0x7f, 0x1e, 0x00, 0x80, 0xfe, 0x1c, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x78, 0x0c, 0x06, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0xc0, 0xc0, 0x80, 0x01, 0x03, 0x1c, 0x70, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0xc0, 0x78, 0x09, 0x01, 0x01, 0x01, 0x01,
0x01, 0x01, 0x01, 0x01, 0x01, 0x09, 0x79, 0xc0, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x76, 0x5f, 0x00, 0x24, 0x25, 0x25,
0x25, 0x2d, 0x2d, 0x6d, 0x00, 0x09, 0x7f, 0x36, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x80, 0x30, 0x38, 0xa8, 0x2c,
0x2c, 0x2c, 0x2c, 0x28, 0x30, 0x20, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};


/**************************************************************************************************
*所有的全局变量
*电压采样值和测频是采样到得个数
*
*
**************************************************************************************************/
uint16_t timeoutCounter;
uint32_t results[10];
uint32_t sum=0,com,acom,flag=0;
uint32_t cap,newdata,olddata,data;
uint32_t num;
uint8_t RTCExitSec = 0;

static const char *const clockMenuText[] = {
"===SDDZ 12XX====",
"-.-",
"1. Start ",
"2. Contrast ",
"3. Backlight "

};

// Forward declared functions
void ContrastSetting(void);
void BacklightSetting(void);
void celiang(void);
void display1();
void display2();

/***************************************************************************//**
* @brief The menu of lab1.
* @param None
* @return none
******************************************************************************/

void lab1(void)
{
uint8_t selection = 0;
buttonsPressed = 0;
Dogs102x6_clearScreen(); //清屏
Dogs102x6_stringDraw(7, 0, "*S1=Enter S2=Esc*", DOGS102x6_DRAW_NORMAL);
selection = Menu_active((char **)clockMenuText, 5); //显示菜单,并返回菜单选项
if (buttonsPressed & BUTTON_S2);
else
switch (selection)
{
case 2: celiang(); break; //数字时钟程序
case 3: ContrastSetting(); break; //对比度设置程序
case 4: BacklightSetting(); break; //背光设置程序
default: break;
}
}
/***************************************************************************//**
测量模块函数
******************************************************************************/
void celiang(void)
{

Dogs102x6_clearScreen();
Board_ledOff(LED_ALL);
ADC12CTL0 |= ADC12SC;
_EINT();

cap=0;
acom=0;
com=0;

P1DIR |= BIT3;
P2SEL |= BIT0; //TA1.1
while (1)
{
buttonsPressed = 0;
Dogs102x6_clearScreen();
while (!(buttonsPressed & BUTTON_S1))
{
//ADC12IE = 0x01;
Board_ledOn(LED4);

TA1CCTL1=CM_1+SCS+CCIS_0+CAP+CCIE;
TA1CTL=TASSEL_2+MC_2+TACLR+TAIE;

display2();
}
buttonsPressed = 0;
Dogs102x6_clearScreen();
__delay_cycles(2000);
Board_ledOff(LED_ALL);


while (!(buttonsPressed & BUTTON_S2))
{
ADC12IE = 0x01;
Board_ledOn(LED6);
display1();
}
Dogs102x6_clearScreen();
__delay_cycles(2000);
Board_ledOff(LED_ALL);
ADC12IE = 0x00;
ADC12CTL0 &= ~ADC12SC;
}
}
/**************************************************************************************************
*直流电压采样数据转换显示
*
*
*
**************************************************************************************************/
void display1()
{
if(flag==1)
{
char string[20];
string[0]=com/1000+48;
string[1]=46;
string[2]=com/100%10+48;
string[3]=com/10%10+48;
string[4]=com%10+48;
string[5]='\0';

Dogs102x6_stringDraw(1, 0, "*==DC voltage==*", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(3, 0, "value=", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(3, 40, string, DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(3, 70, "(V)", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(7, 0, " *== good job==*", DOGS102x6_DRAW_NORMAL);

for (timeoutCounter = 0; timeoutCounter < 0x02FF; timeoutCounter++)
{
__delay_cycles(1000);
}
flag=0;
}
}
/**************************************************************************************************
*交流电压采样数据转化显示
*频率采样显示
*
*
**************************************************************************************************/
void display2()
{
char str1[20],str3[20];

cap=40000000/num;

str1[0]=acom/1000+48;
str1[1]=46;
str1[2]=acom/100%10+48;
str1[3]=acom/10%10+48;
str1[4]=acom%10+48;
str1[5]='\0';


str3[0]=cap/10000000+'0';
str3[1]=cap/1000000%10+'0';
str3[2]=cap/100000%10+'0';
str3[3]=cap/10000%10+'0';
str3[4]=cap/1000%10+'0';
str3[5]=cap/100%10+'0';
str3[6]=cap/10%10+'0';
str3[7]=46;
str3[8]=cap%10+'0';
str3[9]='\0';

Dogs102x6_stringDraw(1, 0, "*==AC voltage==*", DOGS102x6_DRAW_NORMAL);

Dogs102x6_stringDraw(3, 0, "value=", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(3, 40, str1, DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(3, 75, "(V)", DOGS102x6_DRAW_NORMAL);


Dogs102x6_stringDraw(5, 1, "F =", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(5, 30, str3, DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(5, 90, "HZ", DOGS102x6_DRAW_NORMAL);

Dogs102x6_stringDraw(7, 0, " *== good job==*", DOGS102x6_DRAW_NORMAL);

}


/***************************************************************************//**
* @brief Allows the user to adjust the contrast
* @param none
* @return none
******************************************************************************/

void ContrastSetting(void)
{
uint8_t contrast = *((unsigned char *)contrastSetpointAddress);

buttonsPressed = 0;
Dogs102x6_clearScreen();
Dogs102x6_stringDraw(0, 0, " Adjust contrast ", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(1, 0, "by turning wheel.", DOGS102x6_DRAW_NORMAL);

Dogs102x6_imageDraw(sunglasses, 2, 27); //显示太阳镜图案
__delay_cycles(10000000); //delay for user to read directions

while (!buttonsPressed)
{
contrast = Wheel_getValue() / 130; //通过齿轮电位计采样得到需设置的对比度值
Dogs102x6_setContrast(contrast); //重置对比度
}

WriteFlashSettings(contrast, contrastSetpointAddress); //将新对比度值写入FLASH地址 保存设置

buttonsPressed = 0;
Dogs102x6_clearScreen();
}

/***************************************************************************//**
* @brief Allows the user to adjust the backlight brightness
* @param none
* @return none
******************************************************************************/

void BacklightSetting(void)
{
uint8_t brightness = *((unsigned char *)brightnessSetpointAddress);

buttonsPressed = 0;
Dogs102x6_clearScreen();
Dogs102x6_stringDraw(0, 0, "Adjust brightness", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(1, 0, "by turning wheel.", DOGS102x6_DRAW_NORMAL);
Dogs102x6_imageDraw(lightbulb, 2, 35); //显示灯泡图案

while (!buttonsPressed)
{
brightness = Wheel_getValue() / 340; //通过齿轮电位计采样得到需设置的背光参数
if (brightness > 12)
brightness = 12; //背光参数最大为12
Dogs102x6_setBacklight(brightness); //重置背光值
}

WriteFlashSettings(brightness, brightnessSetpointAddress); //将新背光值写入FLASH地址,保存设置

buttonsPressed = 0;
Dogs102x6_clearScreen();
}


/***************************************************************************//**
* @brief Initializes the RTC calendar.
* Initial values are January 01, 2010, 12:30:05
* @param none
* @return none
******************************************************************************/

void SetupRTC(void)
{
RTCCTL01 = RTCMODE + RTCBCD + RTCHOLD + RTCTEV_1;

RTCHOUR = 0x04;
RTCMIN = 0x30;
RTCSEC = 0x00;
RTCDAY = 0x01;
RTCMON = 0x01;
RTCYEAR = 0x2011;

RTCCTL01 &= ~RTCHOLD;

// RTCPS1CTL = RT1IP_5; // Interrupt freq: 2Hz
//RTCPS0CTL = RT0IP_7; // Interrupt freq: 128hz

RTCCTL0 |= RTCRDYIE + RTCTEVIE; // Enable interrupt
}

/***************************************************************************//**
* @brief RTC Interrupt Service Routine. Handles time events.
* @param none
* @return none
******************************************************************************/

#pragma vector=RTC_VECTOR
__interrupt void RTC_ISR(void)
{
switch (__even_in_range(RTCIV, RTC_RT1PSIFG))
{
// Vector RTC_NONE: No Interrupt pending
case RTC_NONE:
break;

// Vector RTC_RTCRDYIFG: RTC ready
case RTC_RTCRDYIFG:
if (RTCExitSec == 1)
__bic_SR_register_on_exit(LPM3_bits);
break;

// Vector RTC_RTCTEVIFG: RTC interval timer
case RTC_RTCTEVIFG:
break;

// Vector RTC_RTCAIFG: RTC user alarm
case RTC_RTCAIFG:
break;

// Vector RTC_RT0PSIFG: RTC prescaler 0
case RTC_RT0PSIFG:
break;

// Vector RTC_RT1PSIFG: RTC prescaler 1
case RTC_RT1PSIFG:
break;

// Default case
default:
break;
}
__no_operation();
}

/***************************************************************************//**
* @brief Writes the settings to flash
* @param Data to be written, and offset
* @return none
******************************************************************************/

void WriteFlashSettings(uint16_t Data, uint16_t Address)
{
uint16_t * Flash_ptr; // Initialize Flash pointer
uint16_t Flash_Contents[16]; // Store Contents of Flash before Programming
uint8_t i;

Flash_ptr = (uint16_t *)(0x1880); // Info C

for (i = 0; i < 16; i++) // We know that we will only use > 8 variables in Info C
{
Flash_Contents[i] = *Flash_ptr; // Read a word from flash
if (Flash_ptr == (uint16_t *)Address)
Flash_Contents[i] = Data;
*Flash_ptr++;
}


Flash_ptr = (uint16_t *)(0x1880); // Info C
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY + ERASE; // Set Erase bit
*Flash_ptr = 0; // Dummy write to erase Flash seg
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation

for (i = 0; i < 16; i++)
{
*Flash_ptr++ = Flash_Contents[i]; // Write a word to flash
}

FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}


/**************************************************************************************************
*ADC12中断函数
*
*
*
**************************************************************************************************/
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
{
switch(__even_in_range(ADC12IV,34))
{
case 0: break; // Vector 0: No interrupt
case 2: break; // Vector 2: ADC overflow
case 4: break; // Vector 4: ADC timing overflow
case 6: // Vector 6: ADC12IFG0
{
static unsigned int m,count = 0;
float factor=0.80566;
results[count]=ADC12MEM0;
count++;
for(m=0;m<10;m++)
{
sum+=results[m];
}
sum/=10;
sum=sum*factor;
com=sum;
if (count == 10)
{
count = 0;
flag=1;
ADC12IE = 0x00;
}
}
case 8: break; // Vector 8: ADC12IFG1
case 10: break; // Vector 10: ADC12IFG2
case 12: break; // Vector 12: ADC12IFG3
case 14: break; // Vector 14: ADC12IFG4
case 16: break; // Vector 16: ADC12IFG5
case 18: break; // Vector 18: ADC12IFG6
case 20: break; // Vector 20: ADC12IFG7
case 22: break; // Vector 22: ADC12IFG8
case 24: break; // Vector 24: ADC12IFG9
case 26: break; // Vector 26: ADC12IFG10
case 28: break; // Vector 28: ADC12IFG11
case 30: break; // Vector 30: ADC12IFG12
case 32: break; // Vector 32: ADC12IFG13
case 34: break; // Vector 34: ADC12IFG14
default: break;
}
}

lab1main:


#include <stdint.h>
#include "msp430.h"
#include "HAL_PMM.h"
#include "HAL_UCS.h"
#include "HAL_Board.h"
#include "HAL_Buttons.h"
#include "HAL_Dogs102x6.h"
#include "HAL_Menu.h"
#include "HAL_Wheel.h"
#include "LPM.h"
#include "PMM.h"
#include "lab1.h"


uint16_t timeoutCounter;

// This image has been created by ImageDog using 'ti_bug.jpg'
static const uint8_t tiBug[] =
{
0x42, // Image width in pixels
0x08, // Image height in rows (1 row = 8 pixels)
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x03, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f,
0x0f, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0x0f, 0x0f, 0x0f, 0x0f, 0x08, 0x00, 0x00, 0x0f, 0xcf, 0xcf, 0xcf, 0xcf,
0xcf, 0xc8, 0x00, 0x00, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f,
0x0f, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xf8, 0xf0, 0xf0, 0xf0, 0xf0, 0xc0, 0x00, 0x07, 0xff, 0xff, 0xff, 0xff,
0xff, 0xfe, 0xc0, 0x00, 0x00, 0xf0, 0xf0, 0xf0, 0xf0, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0x01, 0x00, 0x00, 0x00, 0x70, 0x7c, 0x7e, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f,
0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0x7f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xcf, 0x0f, 0x0f, 0x0f, 0x00, 0x00, 0x01, 0x3f, 0xff, 0xff, 0xff,
0xff, 0xff, 0xf0, 0x00, 0x01, 0x0f, 0x0f, 0x0f, 0x0f, 0x0f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x7f, 0x3f, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0xc0, 0xe0,
0xf0, 0xfc, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xfc, 0x80, 0x00, 0x0e, 0xfe, 0xfe, 0xfe,
0xfe, 0xfe, 0xfc, 0x80, 0x00, 0x0e, 0xfe, 0xfe, 0xfe, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x80, 0xe0, 0xf0, 0xf8, 0xf8, 0xf8, 0xf8, 0xf8, 0xf0, 0xe0, 0xc0, 0x80,
0x80, 0x80, 0xc0, 0xc0, 0xf0, 0xf8, 0xfe, 0xff, 0xff, 0xff, 0xff, 0x03, 0x03, 0x01, 0x01, 0x01,
0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x0f, 0xff, 0xff, 0xff, 0xfe, 0xfe,
0xfc, 0xf8, 0xf0, 0xf0, 0xe0, 0xe0, 0xc0, 0xc0, 0xc0, 0x80, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0xe0, 0xf8, 0xfe, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xf8, 0xe0, 0xc0, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80,
0xc0, 0xf0, 0xf0, 0xf8, 0xfc, 0xfe, 0xfe, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x02, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};

void main(void)
{
uint8_t contrast = *((unsigned char *)contrastSetpointAddress); //读取FLASH中对比度值
uint8_t brightness = *((unsigned char *)brightnessSetpointAddress); //读取FLASH中背光值

// Initialize accelerometer offset from flash
// Cma3000_setAccel_offset(*((unsigned char *)accelXcalibrationAddress), //初始化加速度偏移量
// *((unsigned char *)accelYcalibrationAddress),
// *((unsigned char *)accelZcalibrationAddress));

// Stop WDT
WDTCTL = WDTPW + WDTHOLD; //关闭看门狗

// Basic GPIO initialization
Board_init(); //初始化GPIO

// Set Vcore to accomodate for max. allowed system speed
SetVCore(3); //设VCore为最大

// Use 32.768kHz XTAL as reference
LFXT_Start(XT1DRIVE_0); //利用LFXT1(32.768kHZ)作为时钟参考

// Set system clock to max (25MHz)
Init_FLL_Settle(25000, 762); //利用FLL(锁频环)将系统时钟设为最大25MHZ

SFRIFG1 = 0; //清中断标志
SFRIE1 |= OFIE; //使能晶振失效中断

// Globally enable interrupts
__enable_interrupt(); //使能全局中断

// Setup real time clock
SetupRTC(); //设置实时时钟

// Set up LCD
Dogs102x6_init(); //初始化LCD
Dogs102x6_backlightInit(); //背光初始化

// Contrast not programed in Flash Yet
if (contrast == 0xFF) //若当前FLASH中无对比度值,则将对比度值设为11(默认)
// Set Default Contrast
contrast = 11;

// Brightness not programed in Flash Yet
if (brightness == 0xFF) //若当前FLASH中无背光值,则将背光值设为11(默认)
// Set Default Brightness
brightness = 11;

P6SEL |= BIT6;//P6.6设置为输入口
ADC12CTL0 = ADC12ON+ADC12SHT0_8+ADC12MSC;
ADC12CTL1 = ADC12SHP+ADC12CONSEQ_2;
ADC12MCTL0=ADC12SREF_0+ADC12INCH_6;
ADC12IE |= BIT0;
ADC12CTL0 |= ADC12ENC;
ADC12CTL0|=ADC12SC;

Dogs102x6_setBacklight(brightness); //设置初始背光值
Dogs102x6_setContrast(contrast); //设置初始对比度值
Dogs102x6_clearScreen(); //清屏

// Set up wheel
Wheel_init(); //初始化齿轮电位计
Buttons_init(BUTTON_ALL); //初始化按键
Buttons_interruptEnable(BUTTON_ALL); //使能所有按键中断
buttonsPressed = 0; //键值清零

// Display TI logo
Dogs102x6_imageDraw(tiBug, 0, 16); //显示TI图案

// Wait for button press
while (!buttonsPressed) //等待按键被按下,或者超时退出等待
{
for (timeoutCounter = 0; timeoutCounter < 0xFFFF; timeoutCounter++)
{
if (buttonsPressed)
break;
__delay_cycles(1000);
}

//Timeout break
break; //超时退出
}
Dogs102x6_clearScreen();
buttonsPressed = 0;
//显示文字说明:
Dogs102x6_stringDraw(3, 0, " Welcome to ", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(4, 0, " CE LIANG ", DOGS102x6_DRAW_NORMAL);
Dogs102x6_stringDraw(6, 0, "Wait for a moment", DOGS102x6_DRAW_INVERT);
Dogs102x6_stringDraw(7, 0, "or press S1 | S2 ", DOGS102x6_DRAW_INVERT);

// Wait for button press
while (!buttonsPressed) //等待按键被按下,或者超时退出等待
{
for (timeoutCounter = 0; timeoutCounter < 0xFFFF; timeoutCounter++)
{
if (buttonsPressed)
break;
__delay_cycles(2000);
}

//Timeout break
break;
}
/**************************************************************************************************
*ADC12的初始化
*
*
*
**************************************************************************************************/

// 主循环
while (1)
{
lab1(); //试验一程序
}
}