刚上手的TI原装f5529开发板,为什么Vcc有3.6V呢,不是3.3V,出厂配置就是3.6吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,
是5529的launchpad吗?应该是3.3v的。建议先断开板子右上部的3.3v跳线,测量一下是不是3.3v
是5529的launchpad,你是指JP16那里的DVCC吗?我拿万用表测了J4、J5上的Vcc和GND以及J10上的Vcc和GND,都是3.6V;
所以我的ADC测电压也不准
楼主,
launchpad的5V从USB进来之后经过LDO之后产生3.3V,通过跳线JP2接到MSP430F5529.可以先断掉JP2跳线,直接测量LDO的输出,看看是否是3.3V。