This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5438A的RTC中断问题



为什么程序在RTC中断服务程序里跳不出来,主函数中的while(1)中的语句总也得不到执行!程序如下!

while(1){

         //Set all P1 pins HI

   GPIO_setOutputHighOnPin(

       __MSP430_BASEADDRESS_PORT5_R__,

       GPIO_PORT_P5,

       GPIO_PIN0 + GPIO_PIN1 + GPIO_PIN2 + GPIO_PIN3 +

       GPIO_PIN4 + GPIO_PIN5 + GPIO_PIN6 + GPIO_PIN7

       );

     __delay_cycles(1000000);

       GPIO_setOutputLowOnPin(

       __MSP430_BASEADDRESS_PORT5_R__,

       GPIO_PORT_P5,

       GPIO_PIN0 + GPIO_PIN1 + GPIO_PIN2 + GPIO_PIN3 +

       GPIO_PIN4 + GPIO_PIN5 + GPIO_PIN6 + GPIO_PIN7

       );

     /* if(flag==1)

     {

     flag=0;    

     Send_Hex_1(newTime.Year>>8) ;   delay();delay();

     Send_Hex_1(newTime.Year)   ;    delay();delay();  

     Send_Hex_1(newTime.Month)  ;    delay();delay();  

     Send_Hex_1(newTime.DayOfMonth); delay();delay();  

     Send_Hex_1(newTime.DayOfWeek) ; delay();delay();

     Send_Hex_1(newTime.Hours) ;     delay();delay();  

     Send_Hex_1(newTime.Minutes) ;      

     __delay_cycles(1000000);

     }*/

   //Enter LPM3, interrupts enabled

  __bis_SR_register(LPM3_bits + GIE);

  __no_operation();

   }

#pragma vector=RTC_VECTOR

__interrupt void RTC_ISR (void)

{

   switch (__even_in_range(RTCIV,16)){

       case 0: break;  //No interrupts

       case 2:         //RTCRDYIFG  Read Ready Interrupt flag

           //Toggle P1.0 every second

           GPIO_toggleOutputOnPin(__MSP430_BASEADDRESS_PORT1_R__,

           GPIO_PORT_P1,

           GPIO_PIN0);

           break;

       case 4:         //RTCEVIFG  time event interrupt enable

           //Interrupts every minute

           __no_operation();

           //Read out New Time a Minute Later BREAKPOINT HERE

           newTime = RTC_getCalendarTime(__MSP430_BASEADDRESS_RTC__);

     Send_Hex_1(newTime.Year>>8) ;   delay();delay();

     Send_Hex_1(newTime.Year)   ;    delay();delay();  

     Send_Hex_1(newTime.Month)  ;    delay();delay();  

     Send_Hex_1(newTime.DayOfMonth); delay();delay();  

     Send_Hex_1(newTime.DayOfWeek) ; delay();delay();

     Send_Hex_1(newTime.Hours) ;     delay();delay();  

     Send_Hex_1(newTime.Minutes) ;

           break;

       case 6:         //RTCAIFG  clock alarm interrupt flag

           //Interrupts 5:00pm on 5th day of week

          // __no_operation();

           break;

       case 8: break;  //RT0PSIFG

       case 10: break; //RT1PSIFG

       case 12: break; //Reserved

       case 14: break; //Reserved

       case 16: break; //Reserved

       default: break;

   }

}