This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP5438A的RTC中断服务程序问题



我想从430的串口向PC机发送时间数据,但是程序在中RTC的中断服务程序里跳不出来,在主函数中的程序无法执行,请问是什么问题,急!

#include "zyh.h"

unsigned char flag=0;

unsigned int status;

Calendar newTime;

void main (void)

{

  unsigned char i,*p;

  Calendar currentTime;

 //Setup Current Time for Calendar

   currentTime.Seconds    = 0x00;

   currentTime.Minutes    = 0x08;

   currentTime.Hours      = 0x12;

   currentTime.DayOfWeek  = 0x07;

   currentTime.DayOfMonth = 0x11;

   currentTime.Month      = 0x03;

   currentTime.Year       = 0x2012;

 //Stop WDT

   WDT_hold(__MSP430_BASEADDRESS_WDT_A__);

   Sys_Clock_Init();    //系统时钟初始化

   Serial_1_Init();    //串口初始化

   RTC_A_Calender_Init(currentTime);  //RTC初始?

   p=zyh;

   while(1){    

      if(flag==1)

     {

     flag=0;    

     Send_Hex_1(newTime.Year>>8) ;   delay();delay();//向串口发送时间数据,在PC上显示

     Send_Hex_1(newTime.Year)   ;    delay();delay();  

     Send_Hex_1(newTime.Month)  ;    delay();delay();  

     Send_Hex_1(newTime.DayOfMonth); delay();delay();  

     Send_Hex_1(newTime.DayOfWeek) ; delay();delay();

     Send_Hex_1(newTime.Hours) ;     delay();delay();  

     Send_Hex_1(newTime.Minutes) ;      

     __delay_cycles(1000000);

     }

   //Enter LPM3, interrupts enabled

  __bis_SR_register(LPM3_bits + GIE);

  __no_operation();

   }

}

//整个程序在这个中断服务程序里边跳不出来,无法执行主函数

#pragma vector=RTC_VECTOR

__interrupt void RTC_ISR (void)

{

   switch (__even_in_range(RTCIV,16)){

       case 0: break;  //No interrupts

       case 2:         //RTCRDYIFG  Read Ready Interrupt flag

           //Toggle P1.0 every second

           GPIO_toggleOutputOnPin(__MSP430_BASEADDRESS_PORT1_R__,

           GPIO_PORT_P1,

           GPIO_PIN0);

           break;

       case 4:         //RTCEVIFG  time event interrupt enable

           //Interrupts every minute

           __no_operation();

           //Read out New Time a Minute Later BREAKPOINT HERE

           newTime = RTC_getCalendarTime(__MSP430_BASEADDRESS_RTC__);

     Send_Hex_1(newTime.Year>>8) ;   delay();delay();

     Send_Hex_1(newTime.Year)   ;    delay();delay();  

     Send_Hex_1(newTime.Month)  ;    delay();delay();  

     Send_Hex_1(newTime.DayOfMonth); delay();delay();  

     Send_Hex_1(newTime.DayOfWeek) ; delay();delay();

     Send_Hex_1(newTime.Hours) ;     delay();delay();  

     Send_Hex_1(newTime.Minutes) ;

           break;

       case 6:         //RTCAIFG  clock alarm interrupt flag

           //Interrupts 5:00pm on 5th day of week

          // __no_operation();

           break;

       case 8: break;  //RT0PSIFG

       case 10: break; //RT1PSIFG

       case 12: break; //Reserved

       case 14: break; //Reserved

       case 16: break; //Reserved

       default: break;

   }

}

//******************************************************************************

//

//This is the USCI_A0 interrupt vector service routine.

//

//******************************************************************************

#pragma vector=USCI_A0_VECTOR

__interrupt void USCI_A0_ISR (void)

{

   switch (__even_in_range(UCA0IV,4)){

       //Vector 2 - RXIFG

       case 2:

           //Echo back RXed character, confirm TX buffer is ready first

           //USCI_A0 TX buffer ready?

           while (!UART_getInterruptStatus(__MSP430_BASEADDRESS_USCI_A0__,

                      UART_TRANSMIT_INTERRUPT_FLAG)

                  ) ;

           //Receive echoed data//将接收到的字符串存到缓存中

          Buf_First_Serial[First_Int]= UART_receiveData(__MSP430_BASEADDRESS_USCI_A0__);            

First_Int++;                 //缓存指针向后移动

if(First_Int > Buf1_Max)       //如果缓存满,将缓存指针指向缓存的首地址

{

First_Int = 0;

}

           break;

       default: break;

   }

}

/*-----------------------------------------------------------------------------

Fun name :

Parameter:

Descripe :系统时钟设置中断函数

-------------------------------------------------------------------------------*/

#pragma vector=UNMI_VECTOR

__interrupt void NMI_ISR(void)

{

 do {

   // If it still can't clear the oscillator fault flags after the timeout,

   // trap and wait here.

   status = UCS_clearAllOscFlagsWithTimeout(__MSP430_BASEADDRESS_UCS__,

                                            1000

                                            );

 } while(status != 0);

}