This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[求助]关于MSP430F5529的DCO部分



Hello.

先说说我对DCO这一块的理解吧。DCO最终输出的频率可以有两种不同的方式控制(相同的DCORSEL下),一种是关闭FLL,软件设置UCSCTL0的DCO来确定最终输出的频率;另一种是使能FLL,由硬件来调节输出频率。

这边有点问题:

1.以上两种调节之间有联系吗?使能FLL时的硬件调节与UCSCTL0的DCO和MOD有关系吗?

2.UCSCTL0还有个MOD,调制位计数器,既然作为一个计数器,那它什么时候自加,或者什么时候自减?

3.如果关闭调制器(UCSCTL1的DISMOD置位),在关闭FLL和开启FLL的情况下各有什么影响?

4.关闭了FLL后,通过改变UCSCTL0的DCO来控制输出频率,资料说选择的频拍,应该是指一个频率范围吧?但是示波器观测的是一个较稳定的频率值(P7.7口)。

希望能尽快得到解答!谢谢!