This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于msp430ADC12的问题,采集不到低电压

Other Parts Discussed in Thread: MSP430F149

我做的一个采样测试,基准电压用的是内部的2.5v,采样自己制作的滑动变阻器的电压,再经过串口发送到PC机上显示,但是测试时候只能采集到大概1V以上的电压,对于1V以下的电压它就不采集了,也不发送了,PC机在小于1V的电压时没有接受到采样数据,这个实在怎么回事啊,不会是430单片机不能采集1V一下的电压信号?我用的是MSP430F149,请各位大神指导指导,急。。。。。。。。。

  • 不要着急,你要系统的了解430的ADC外设

    ****************************************************************

    MSP430F149的ADC12模块

    1 概述

      MSP430F149的ADC12为SAR型12位AD,共有16路输入通道,其中8路独立的外部输入通道,2路接外部Vref+,Vref-,3路内部通道可分别测内部温度传感器、AVCC、和外部参考源。

        P6口第二功能为AD输入端。MSP430F149的10、11分别接外部电压参考源正负极,7脚可将内部电压参考源输出。

        ADC12共有18个中断源,公用一个中断向量ADC12_VECTOR。

    AD的参考源可选择内部电压参考源或外部电压参考源。内部电压参考源有1.5V,2.5V可选,使用时向ADC12CTL0写入REFON+ REF2_5V就打开了2.5V。外部电压参考源由REF+接入。上电时若不设置参考源,则参考源为系统供电电压3.3V。

    2 使用方法概述

    2.1程序架构

    中断方式

        1、设置  ADC12工作模式,启动转换,开全局中断,等待中断

        2、写中断处理函数

    查询方式

        设置ADC12工作模式,启动转换,查询中断标志ADC12IFG

        while (!(0x01 & ADC12IFG));转换完毕读取采样值,系统自动清除中断标志

    2.2 使用概述

    主要参数配置

     设置工作方式:sing\\sequence\\re-sing\\re-sequencd;

     设置转换时间:SHTX

     设置触发方式:ADC12SC\\MSC\\TimerA\\ TimerB

     设置通道:外部通道\\内部Temperature sensor

     设置参考源:系统电压\\内部参考源\\外部参考源

    其他细节配置

         一般要配置采样转换模式为脉冲(SHP),打开ADC12(ADC12ON),使能ADC12转换(ENC),使能中断(如果采取中断模式),触发转换(若采用ADC12SC触发)。

    解释

     ADC12模数转换是在SHI的上升沿初始化的。SHI信号有四个来源: The ADC12SC bit;The Timer_A Output Unit 1; The Timer_B Output Unit 0; The Timer_B Output Unit 1。故单次采样时只需要每次设置ADC12CTL0 |= ADC12SC就采样一次;重复采样时,如Rep-sing,设置ADC12CTL1 = SHS_1 +CONSEQ_2就选择了Rep-sing模式,每次采样通过定时器A触发。

    3 相关寄存器

    1、ADC12CTL0

    SHT1x Bits

    Sample-and-hold time. These bits define the number of ADC12CLK cycles in

    the sampling period for registers ADC12MEM8 to ADC12MEM15.

    SHT0x Bits

    Sample-and-hold time. These bits define the number of ADC12CLK cycles in

    the sampling period for registers ADC12MEM0 to ADC12MEM7.

    ADC12ON

    0 ADC12 off

    1 ADC12 on

    ENC

    ENC Bit 1 Enable conversion

    0 ADC12 disabled

    1 ADC12 enabled

    ADC12SC Bit 0 Start conversion. Software-controlled sample-and-conversion start.

    ADC12SC and ENC may be set together with one instruction. ADC12SC is

    reset automatically.

    0 No sample-and-conversion-start

    1 Start sample-and-conversion

    MSC Bit 7 Multiple sample and conversion. Valid only for sequence or repeated modes.

    0 The sampling timer requires a rising edge of the SHI signal to trigger

    each sample-and-conversion.

    1 The first rising edge of the SHI signal triggers the sampling timer, but

    further sample-and-conversions are performed automatically as soon

    as the prior conversion is completed.

    2、ADC12CTL1

    SHP

    SHP Bit 9 Sample-and-hold pulse-mode select. This bit selects the source of the

    sampling signal (SAMPCON) to be either the output of the sampling timer or

    the sample-input signal directly.

    0 SAMPCON signal is sourced from the sample-input signal.

    1 SAMPCON signal is sourced from the sampling timer.

    SHSx Bits

    11-10

    Sample-and-hold source select

    00 ADC12SC bit

    01 Timer_A.OUT1

    10 Timer_B.OUT0

    11 Timer_B.OUT1

    CONSEQx Bits

    2-1

    Conversion sequence mode select

    00 Single-channel, single-conversion

    01 Sequence-of-channels

    10 Repeat-single-channel

    11 Repeat-sequence-of-channels

    3、ADC12IE

    ADC12IEx Bits

    15-0

    Interrupt enable. These bits enable or disable the interrupt request for the ADC12IFGx bits.

    0 Interrupt disabled

    1 Interrupt enabled

    4、ADC12IFG

    ADC12IFGx Bits

    15-0

    ADC12MEMx Interrupt flag. These bits are set when corresponding

    ADC12MEMx is loaded with a conversion result. The ADC12IFGx bits are

    reset if the corresponding ADC12MEMx is accessed, or may be reset with

    software.

    0 No interrupt pending

    1 Interrupt pending

    5、ADC12MCTLX

    SREFx Bits

    6-4

    Select reference

    000 VR+ = AVCC and VR− = AVSS

    001 VR+ = VREF+ and VR− = AVSS

    010 VR+ = VeREF+ and VR− = AVSS

    011 VR+ = VeREF+ and VR− = AVSS

    100 VR+ = AVCC and VR− = VREF−/ VeREF−

    101 VR+ = VREF+ and VR− = VREF−/ VeREF−

    110 VR+ = VeREF+ and VR− = VREF−/ VeREF−

    111 VR+ = VeREF+ and VR− = VREF−/ VeREF−

    INCHx Bits

    3-0

    Input channel select

    0000 A0

    0001 A1

    0010 A2

    0011 A3

    0100 A4

    0101 A5

    0110 A6

    0111 A7

    1000 VeREF+

    1001 VREF−/VeREF−

    1010 Temperature sensor

    1011 (AVCC – AVSS) / 2

    1100 (AVCC – AVSS) / 2

    1101 (AVCC – AVSS) / 2

    1110 (AVCC – AVSS) / 2

    1111 (AVCC – AVSS) / 2

    EOS Bit 7 End of sequence. Indicates the last conversion in a sequence.

    0 Not end of sequence

    1 End of sequence

    4实例

    4.1 single采样,参考电源为系统电源

    1.设置ADC12CTL0,使ADC12通道0采样保持时间为16 ADC12CLK(SHT0_2),开启ADC12模块(ADC12ON);

    2.设置ADC12CTL1,选择采样保持脉冲模式即SAMPCON为采样定时器(SHP)

    3.设置ADC12IE,是通道0中断使能(0x01);

    4.设置ADC12CTL0,使能AD转换(ENC)

    5.设置模拟信号输入IO口P60

    7.设置ADC12CTL0,开启AD转换(ADC12SC),等待中断

    8.中断中读取通道0转换值ADC12MEM0

      ADC12CTL0 = SHT0_2 + ADC12ON;             // Set sampling time, turn on ADC12

      ADC12CTL1 = SHP;                          // Use sampling timer

      ADC12IE = 0x01;                           // Enable interrupt

      ADC12CTL0 |= ENC;                         // Conversion enabled

      P6SEL |= 0x01;                            // P6.0 ADC option select

      P2DIR |= 0x01;

    ADC12CTL0 |= ADC12SC;

    #pragma vector=ADC12_VECTOR

    __interrupt void ADC12_ISR (void)

    {

        if (ADC12MEM0 < 0x7FF)

          P2OUT = 0;                       // Clear P1.0 LED off

        else

          P2OUT = 0XFF;                        // Set P1.0 LED on

        __low_power_mode_off_on_exit();

        // 与上面等价_BIC_SR_IRQ(CPUOFF);                    // Clear CPUOFF bit from 0(SR)

    }

    4.2 single采样参考源为2.5V

    在ADC12CTL0中设置参考源

    在ADC12MCTL0中为通道0选择参考源

      ADC12CTL0 = ADC12ON+SHT0_2+REFON+REF2_5V; // Turn on and set up ADC12

      ADC12CTL1 = SHP;                          // Use sampling timer

      ADC12MCTL0 = SREF_1;                      // Vr+=Vref+

      for ( i=0; i<0x3600; i++);                  // Delay for reference start-up

      ADC12CTL0 |= ENC;  

      while (1)

      {

        ADC12CTL0 |= ADC12SC;                   // Start conversion

        while ((ADC12IFG & BIT0)==0);

        _NOP();                                 // SET BREAKPOINT HERE

      }

    4.3 Repeat-single采样,模拟输入为内部Temperature sensor

    设置ADC12CTL1,采样保持源为定时器A,脉冲保持模式,Repeat-single模式

      ADC12CTL1 = SHS_1 + SHP + CONSEQ_2;       // TA trig., rpt conv.

    设置ADC12MCTL0,通道0参考源为内部REF,模拟输入通道0选择为Temperature sensor

      ADC12MCTL0 = SREF_1 + INCH_10;            // Channel A10, Vref+

      ADC12IE = 0x01;                           // Enable ADC12IFG.0

      ADC12CTL0 = SHT0_8 + REF2_5V + REFON + ADC12ON + ENC; // Config ADC12

      TACCTL1 = OUTMOD_4;                       // Toggle on EQU1 (TAR = 0)

      TACTL = TASSEL_2 + MC_2;                  // SMCLK, cont-mode

      while (!(0x01 & ADC12IFG));               // First conversion?

      FirstADCVal = ADC12MEM0;                  // Read out 1st ADC value

      _BIS_SR(LPM0_bits + GIE);                 // Enter LPM0 w/ interrupt

    #pragma vector=ADC12_VECTOR

    __interrupt void ADC12ISR (void)

    {

      if (ADC12MEM0 <= FirstADCVal + ADCDeltaOn)

          P1OUT &= ~0x01;                       // LED off

      else P1OUT |= 0x01;                       // LED on

    }

    摄氏温度和温度传感器电压转换关系:0摄氏度对应986mv,1摄氏度温差对应1.97mv温差

    //  oF = ((x/4096)*1500mV)-923mV)*1/1.97mV = x*761/4096 - 468

    //  IntDegF = (ADC12MEM0 - 2519)* 761/4096

        IntDegF = (temp - 2519) * 761;

        IntDegF = IntDegF / 4096;

    //  oC = ((x/4096)*1500mV)-986mV)*1/3.55mV = x*423/4096 - 278

    //  IntDegC = (ADC12MEM0 - 2692)* 423/4096

        IntDegC = (temp - 2692) * 423;

        IntDegC = IntDegC / 4096;

    4.4 Repeat-sequence mode

    Sequence模式时可以设置多个采样通道。在最后一个通道加上EOS就表明的采样通道结束位置。中断允许只需要设置最后一个通道。

    为了采样速率尽可能快,可设置MSC,此时当SHI上升沿触发第一次采样后,后面的采样在上一次采样结束后自动进行。

      ADC12CTL0 = ADC12ON+MSC+SHT0_8;           // Turn on ADC12, extend sampling time

                                                // to avoid overflow of results

      ADC12CTL1 = SHP+CONSEQ_3;                 // Use sampling timer, repeated sequence

      ADC12MCTL0 = INCH_0;                      // ref+=AVcc, channel = A0

      ADC12MCTL1 = INCH_1;                      // ref+=AVcc, channel = A1

      ADC12MCTL2 = INCH_2;                      // ref+=AVcc, channel = A2

      ADC12MCTL3 = INCH_3+EOS;                  // ref+=AVcc, channel = A3, end seq.

      ADC12IE = 0x08;                           // Enable ADC12IFG.3

      ADC12CTL0 |= ENC;                         // Enable conversions

      ADC12CTL0 |= ADC12SC;                     // Start conversion

      _BIS_SR(LPM0_bits + GIE);                 // Enter LPM0, Enable interrupts

    #pragma vector=ADC12_VECTOR

    __interrupt void ADC12ISR (void)

    {

      static unsigned int index = 0;

      A0results[index] = ADC12MEM0;             // Move A0 results, IFG is cleared

      A1results[index] = ADC12MEM1;             // Move A1 results, IFG is cleared

      A2results[index] = ADC12MEM2;             // Move A2 results, IFG is cleared

      A3results[index] = ADC12MEM3;             // Move A3 results, IFG is cleared

      index = (index+1)%Num_of_Results;         // Increment results index, modulo; Set Breakpoint here

    }

  • MSP430FR599的ADC在Repeat-Sequence-of-Channels模式下,在转换完最后一个通道时不会自动停止,反而会一直在各个通道循环转换,最后一个通道也加上EOS了,不知为什么?

    我的应用是用TA0产生PWM触发转换序列通道,也设置了ADC12MSC,设想是PWM触发第一个通道,在第一个通道完成后MSC会触发下一个通道,依次进行到最后一个通道,最后一个通道设置的EOS,停止转换,等到下一个PWM脉冲到来时,进行下一次的序列转换。

    实际测试发现,EOS不会停止,为什么?