This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的设备是MSP EXP430 LaunchPad, 芯片是msp430g2553, 我正在尝试通过UART的方式与PC端进行通信,我相信我的数据已经成功放到UCA0TXBUF里面了,可是在PC端却没有办法接收到数据。我已经尝试了Teraterm,CCS6里面的terminal以及其他第三方的终端都接收不到数据。请问这是为什么?我在终端的接收配置也是8-n-1,9600,应该是没有问题的吧。
如果觉得麻烦能够直接给我一个可以成功和PC通信的uart example吗?
谢谢
以下是我的代码:
#include <msp430.h> #include "stdint.h" #include <stdio.h> static const RXBUF_SIZE = 16; static const TXBUF_SIZE = 16; static const uint8_t ch = 'a'; int g = 0; int tmp; char tmp2; unsigned char RX_BUFF[RXBUF_SIZE] = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 }; //receive buffer unsigned int UART_InLen = 16; //input data lenth unsigned char TX_BUFF[TXBUF_SIZE] = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 }; // unsigned int UART_OutLen = 16; //data length unsigned int TX_IndexR = 0; //FIFO pointer for RX unsigned int TX_IndexW = 0; //FIFO pointer for WX unsigned char *str = "helloworld!!!!!"; void main(void) { MCU_init(); LED_init(); UART_init(); UART_sent(ch); _delay_cycles(10); UART0_PutFrame(str,16); int temp = 0; } void MCU_init(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT BCSCTL1 = CALBC1_1MHZ; // Set range DCOCTL = CALDCO_1MHZ; BCSCTL2 &= ~(DIVS_3); // SMCLK = DCO = 1MHz _BIS_SR(GIE); // Enable global interrupt } void UART_init(void) { UCA0CTL1 |= UCSWRST; UCA0CTL1 |= UCSSEL_2; //SMCLK UCA0BR0 = 0x68; //32.768/9600= UCA0BR1 = 0x00; // 1000kHz/9600 = 104.166 =0X68 波特率9600 UCA0MCTL = UCBRS_2; // Modulation UCBRSx = 1 UCA0CTL0 &= ~UCPEN; UCA0CTL0 &= ~UCSPB; UCA0CTL0 &= ~UC7BIT; UCA0CTL1 &= ~UCSWRST; P1SEL |= BIT1 + BIT2; P1SEL2 |= BIT1 + BIT2; //P1DIR |=BIT2; //dont need to configure output in this pin? IFG2 &= ~UCA0TXIFG; IE2 |= UCA0RXIE + UCA0TXIE; unsigned int j; for (j = 0; j < 2000; j++) ; } /* * Put data into buffer and enable the interruption */ int UART0_PutFrame(unsigned char *Ptr, unsigned int Lenth) { int i; if (IE2 & UCA0TXIE) { return (0); } if (Lenth > TXBUF_SIZE) { return (0); } for (i = 0; i < Lenth; i++) { TX_BUFF[i] = Ptr[i]; } TX_IndexR = 0; UART_OutLen = Lenth; IFG2 |= UCA0TXIFG; IE2 |= UCA0TXIE; return (1); } /* * try to send one char */ void UART_sent(uint8_t Chr) { IFG2 &= ~UCA0TXIFG; UCA0TXBUF = Chr; while ((IFG2 & UCA0TXIFG) == 0) ; // USCI_A0 TX buffer ready? } /* * ISR of TX */ #pragma vector=USCIAB0TX_VECTOR __interrupt void USCI0TX_ISR(void) { if (UART_OutLen > 0) { UART_OutLen--; UCA0TXBUF = TX_BUFF[TX_IndexR]; while (!(IFG2 & UCA0TXIFG)); //USCI_A0 TX buffer ready? if (++TX_IndexR >= TXBUF_SIZE) { TX_IndexR = 0; } } else IE2 &= ~UCA0TXIE; } |