活动期间买了MSP430FR5969 LaunchPad开发板,但是Arduino开发环境Energia无法下载程序,提示更新固件,更新后还是无法下载程序,看提示好像驱动有问题,各位使用过这个环境吗?遇到过问题没有。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
活动期间买了MSP430FR5969 LaunchPad开发板,但是Arduino开发环境Energia无法下载程序,提示更新固件,更新后还是无法下载程序,看提示好像驱动有问题,各位使用过这个环境吗?遇到过问题没有。
错误代码如下:
MSPDebug version 0.20 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2012 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
MSP430_GetNumberOfUsbIfs
MSP430_GetNameOfUsbIf
Found FET: COM5
MSP430_Initialize: COM5
FET firmware update is required.
Starting firmware update (this may take some time)...
Initializing bootloader...
Programming new firmware...
20 percent done
40 percent done
60 percent done
80 percent done
100 percent done
100 percent done
Update complete
Done, finishing...
MSP430_VCC: 3000 mV
MSP430_OpenDevice
tilib: MSP430_OpenDevice: Unknown device (error = 5)
tilib: device initialization failed