This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:关于MSP430G255310位ADC的采样问题

Other Parts Discussed in Thread: MSP430G2553

那天写了一个ADC转换的问题,通过A0通道采样。把P1.0设置为输入,但ADC10CTL0 |= ADC10SC;这条语句一执行。P1.0就有电压了,本来应该是0伏特。如果把那条语句屏蔽了,P1.0就是0V。给P1.0配置下拉电阻,不采集的时候是0,但采集时误差太大了。各位大神能帮我看下问题出在哪儿了吗?谢谢!程序代码如下:

#include <msp430g2553.h>

#define uint unsigned int

 #define uchar unsigned char

 #define Num_of_Results 32

 static uint results[Num_of_Results]; /*宏定义各端口,RS(CS)串行通信片选,SID(R/W)串行数据口,SCLK(E)串行同步时钟信号*/

#define RS_0 P2OUT &= ~BIT0     //RS = 0

#define RS_1 P2OUT |= BIT0      //RS = 1

#define SID_0 P2OUT &= ~BIT1    //SID = 0

#define SID_1 P2OUT |= BIT1     //SID = 1

#define SCLK_0 P2OUT &= ~BIT2   //SCLK = 0

#define SCLK_1 P2OUT |= BIT2    //SCLK = 1

uchar m;

unsigned long temp, IntDegF, IntDeg;

void ADC10_init()

 {

   ADC10CTL0 &= ~ENC;

   ADC10CTL0 = ADC10IE+ADC10ON+ADC10SHT_2+MSC+SREF_2;   //ADC10ON开启10ADC

   ADC10CTL1 = CONSEQ_2+INCH_0

;   ADC10AE0 |= 0X03;

   ADC10SA = 0X200;

   __delay_cycles(30000);

   ADC10CTL0 |= ENC;

   ADC10CTL0 |= ADC10SC;

   ADC10CTL0 &= ~ADC10IFG;

   _EINT();

   //LPM0;

}

/*--------------------------------------------

delay_1ms(): 延时函数

 输入参数:无

 编写日期:20140722

  ---------------------------------------------*/

void delay_1ms()

 {  

   uint k;

   for(k=0; k<195; k++);

 }

/*--------------------------------------------

delay(uint n): 延时函数,延时大约1ms

 输入参数:n 延时nms

编写日期:20140722

  ---------------------------------------------*/

 void delay1ms(uint n)

 {   uint j;   for(j=0; j<n; j++)     delay_1ms(); }

/*写指令函数*/

 void write_cmd(uchar cmd)

{

   uchar j;

   j = 0xF8;

   RS_1;             //RS=1

   SCLK_0;            //SCLK=0(E)

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;       //SID(RW)

     else        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   j = cmd;

   j &= 0xF0;

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;

     else

        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   j = cmd;

   j <<= 4;

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;

     else

        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   RS_0;

   delay1ms(5);

 }

/*写显示数据函数*/

 void write_data(uchar dat)

 {

   uchar j;

   j = 0xFA;

   RS_1;

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;

     else

        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   j = dat;

   j &= 0xF0;

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;

     else

        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   j = dat;

   j <<= 4;

   for(m=0; m<8; m++)

   {

     if(j&0x80)          //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0

       SID_1;

     else

        SID_0;    //最高位不为1,写0

     SCLK_0;      //让SCLK产生下降沿,使液晶采样

     delay1ms(1);

     SCLK_1;       //将SCLK拉高,为一位数据采样做准备

     j=j<<1;            //因为先发送高位,所以每次向左移动一位

   }

   RS_0;

   delay1ms(5); }

/*设定显示位置*/

 void lcd_pos(uchar X, uchar Y)

{

   uchar pos;

   if(X == 0)

     X = 0x80;

   else if(X == 1)

     X = 0X90;

   else if(X == 2)

     X = 0X88;

   else if(X == 3)

     X = 0X98;

   pos = X+Y;

   write_cmd(pos);      //显示地址

 }

/*LCD初始化设定*/

 void lcd_init()

 {

   //P1OUT &= ~BIT3;

   //PSB = 1;并口方式

   write_cmd(0x30); //基本指令操作

   delay1ms(5);

   write_cmd(0x0c); //显示开,关光标

   delay1ms(5);

   write_cmd(0x01); //清除LCD的显示类容

   delay1ms(5); }

/*--------------------------------------------

 Init_Port(): MSP430G2553端口初始化函数

 输入参数:无

 编写日期:20140722

  ---------------------------------------------*/

 void Init_Port()

{

    P1DIR = 0;          //将P1口所有的管脚在初始化的时候设置为输入方式

   P2DIR = 0;          //将P2口所有的管脚在初始化的时候设置为输入方式

   //P1REN |= BIT0;

   //P1OUT &= ~BIT0

;   P1SEL |= BIT0;          //将P1口所有的管脚设置为一般I/O口

   P1DIR &= ~BIT0;

   P1DIR |= BIT4;

   P2SEL = 0X00;

   P2IE = 0X00;

   P2DIR = 0XFF;       //将P2口所有的管脚在初始化的时候设置为输入方式

 }

void display(long date)

{

   uchar ge, shi, bai, qian;

   qian=date/1000;

   bai=date%1000/100;

   shi=date%1000%100/10;

   ge=date%1000%100%10;

   lcd_pos(0,2);

   write_data(0x30+qian);

   write_data(0x30+bai);

   lcd_pos(0,3);

   write_data(0x30+shi);

   write_data(0x30+ge);

 }

void main()

 {

   WDTCTL = WDTPW + WDTHOLD;

   BCSCTL1 = CALBC1_8MHZ;

   DCOCTL = CALDCO_8MHZ;

   Init_Port();

   lcd_init();

   ADC10_init();

   while(1);

   }

#pragma vector = ADC10_VECTOR

 __interrupt void ADC10ISR()

{

   uchar i;

   P1DIR |= BIT4;

   P2DIR |= BIT0+BIT1+BIT2;

   static uint index = 0;

   results[index++] = ADC10MEM;

   if(index >= Num_of_Results)

   {

     unsigned long sum = 0;

    index = 0;

    for(i = 0; i < Num_of_Results; i++)

     {

         sum += results[i];

     }

     sum >>= 5;                            //除以32

     temp = 3300*sum/1023;

     display(temp);

   }

 }

  • hongbin deng,

    管脚设置为ADC输入的话,就直接是ADC输入了,不需要使能上下拉电阻。

    建议你直接先用TI提供的code example测试一下,看看可以正确采到电压值否?

    如下为TI 提供关于ADC的群补例程列表,如有有MSP430Ware的话,下列路径可找到,C:\ti\msp430\MSP430ware_1_80_01_03\examples\devices\2xx\MSP430G2xx3_Code_Examples\C

    如果没有的话,可从官网上下载,主页搜MSP430G2553,点进去后Tools & software的softeware部分可以看到,如下。

    MSP430G2x53, MSP430G2x33, MSP430G2x13, MSP430G2x03 Code Examples (Rev. C)  (ZIP 464 KB )    3,673 views, 23 May 2013

    msp430g2x33_adc10_01.c ADC10, Sample A0, Set P1.0 if A0 > 0.5*AVcc
    msp430g2x33_adc10_02.c ADC10, Sample A1, 1.5V Ref, Set P1.0 if A1 > 0.2V
    msp430g2x33_adc10_03.c ADC10, ADC10, Sample A10 Temp, Set P1.0 if Temp ++ ~2C
    msp430g2x33_adc10_04.c ADC10, ADC10, Sample A1, Signed, Set P1.0 if A1 > 0.5*AVcc
    msp430g2x33_adc10_05.c ADC10, ADC10, Sample A11, Lo_Batt, Set P1.0 if AVcc < 2.3V
    msp430g2x33_adc10_06.c ADC10, ADC10, Output Internal Vref on P1.4 & ADCCLK on P1.3
    msp430g2x33_adc10_07.c ADC10, DTC Sample A1 32x, AVcc, Repeat Single, DCO
    msp430g2x33_adc10_08.c ADC10, ADC10, DTC Sample A1 32x, 1.5V, Repeat Single, DCO
    msp430g2x33_adc10_09.c ADC10, ADC10, DTC Sample A10 32x, 1.5V, Repeat Single, DCO
    msp430g2x33_adc10_10.c ADC10, ADC10, DTC Sample A3-01, AVcc, Single Sequence, DCO
    msp430g2x33_adc10_11.c ADC10, ADC10, Sample A1, 1.5V, TA1 Trig, Set P1.0 if > 0.5V
    msp430g2x33_adc10_12.c ADC10, Sample A7, 1.5V, TA1 Trig, Ultra-Low Pwr
    msp430g2x33_adc10_13.c ADC10, DTC Sample A1 32x, AVcc, TA0 Trig, DCO
    msp430g2x33_adc10_14.c ADC10, DTC Sample A1-0 16x, AVcc, Repeat Seq, DCO
    msp430g2x33_adc10_16.c ADC10, ADC10, DTC Sample A0 -> TA1, AVcc, DCO
    msp430g2x33_adc10_temp.c ADC10, Sample A10 Temp and Convert to oC and oF