This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2132 ADC10 采样不准



       用2132的AD口采温度传感器的值,采样值与AD口实际电压值(万用表测量)不一致,有的板子偏高,有的偏低,用的是内部2.5V基准电压。之前用另一款温度传

感器也碰到过这个问题,但把采样周期(sample-and-hold time)加大后就能改好,但新传感器这样改没什么效果,也改了很多其他设置,都没什么效果,请高手指

导一下。

  • 你好,

    你指的精度要求不高,偏差有多少?

    另外你可以把内部2.5V电压做输出,你会发现内部电压其实不止2.50V整,需要算法校正参考原电压。

    或者使用外部参考源,这样精度会大幅提升。