This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS编译F5329代码问题



对于430中的硬件中断程序,采用TI自带的编译器可以编译通过,但是如果采用GNU的GCC编译器,就会报错,程序及报错信息如下:

程序:

#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
{   
    switch(__even_in_range(UCA1IV,0x08))
    {
      case 0: break; // Vector 0 - no interrupt
     
      case 2:  // Vector 2 - RXIFG
        if(bytesAvail > sizeof(uartRXBuf))
        {
            bytesAvail = 0;
        }
        uartRXBuf[bytesAvail] = UCA1RXBUF;
        bytesAvail++;       
        runUARTTerminal();
        break;
   case 4: // Vector 4 - TXIFG
    break;
  
      default:
        break;       
    }
}

 

报错信息:

../board/outerUart.c:124:0: warning: ignoring #pragma vector  [-Wunknown-pragmas]
 #pragma vector=USCI_A1_VECTOR
 ^
../board/outerUart.c:125:13: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'void'
 __interrupt void USCI_A1_ISR(void)
             ^
../board/outerUart.c: In function 'uartRXByte':

请提供解决办法