This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430F149使用中出现的问题,麻烦帮我解答下。



我用430的ADC12输入端接了4路的模拟量作为数据采集端,然后经过AD序列通道转换成数字量发给上位机监测,或者传给另外一个MCU,整体的思想是这些。现在的问题是:我现在先模拟了一路模拟量送给430单片机后,经过AD处理也都好着呢,然后我就通过UART0发送给上位机--串口助手,上面的接收也好着,可是我的设想是当上位机接收到数据后,我人为的在上面给下位机430单片机回执一个“确认信息”,比如在串口助手软件发送口输入个“recept”后显示在下位机的1602液晶上面,可是下位机就是接收不成功????我把接收函数写在了接收中断里面的,麻烦帮我解决下了~~~~~~当我单独调试上位机给下位机发数据然后显示在1602上面时都好着呢,但是接收和发送写在一块的时候,就出问题了。

/****************************************************/
   //通信格式:N.8.1,  9600
  // BCSCTL1 &= ~XT2OFF;                 //打开XT2高频晶体振荡器
  //   do
  //  {
  //       IFG1 &= ~OFIFG;                 //清除晶振失败标志
 //       for (i = 0xFF; i > 0; i--);     //等待8MHz晶体起振
 //   }
 //   while ((IFG1 & OFIFG));             //晶振失效标志仍然存在
 //  BCSCTL2 |= SELM_2 + SELS;           //MCLK和SMCLK选择高频晶振
/*****************************************************/
#include <msp430x14x.h>
#include "cry1602.h"
#include "BoardConfig.h"
#define CPU_F ((double)8000000) //本征函数
#define delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))
#define   Num_of_Results   32
uchar shuzi[] = {"0123456789."};
uchar tishi[] = {"The thic is:"};//浓度指示语句
uchar pX=0,pY=1;
unsigned char Rindex=0;    //数据指针
unsigned char RecBuf[3]; //数据缓冲区
static uint results[Num_of_Results];    //保存ADC转换结果的数组                                                    

void Trans_val(uint Hex_Val);
void PutString(uchar *ptr);
void PutChar(uchar zifu);
/*******************主函数*******************/
void main(void)

  
    uchar *Tishi = " current smoking thickness:";
    P6DIR|=BIT7;
    P6OUT|=BIT7;
    BoardConfig(0xb8);
    WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
    DCOCTL = DCO0 + DCO1 + DCO2;              // Max DCO
    BCSCTL1 = RSEL0 + RSEL1 + RSEL2;          // XT2on, max RSEL
    BCSCTL2 |= SELS;                          // SMCLK = XT2
   
    P3SEL |= 0x30;                            // P3.4,5 = USART0 TXD/RXD
    ME1 |= URXE0 +UTXE0;                      // Enable USART0 TXD/RXD
    UCTL0 |= CHAR;                            // 8-bit character
    UTCTL0 |= SSEL0;                          // UCLK = ACLK
    UBR00 = 0x03;                             // 32k/9600 - 3.41
    UBR10 = 0x00;                             //
    UMCTL0 = 0x4A;                            // Modulation
    UCTL0 &= ~SWRST;                          // Initialize USART state machine
    IE1 |= URXIE0;                            // 使能USART0的接收中断
   
    PutString(Tishi);
    P6SEL |= 0x01;                            // 使能ADC通道
    ADC12CTL0 = ADC12ON +SHT0_8+MSC;           // 打开ADC,设置采样时间
    ADC12CTL1 = SHP+CONSEQ_2;                 // 使用采样定时器
    //ADC12MCTL0 = INCH1;
     ADC12IE   = 0x01;                           // 使能ADC中断
    ADC12CTL0 |= ENC;                         // 使能转换
    ADC12CTL0 |= ADC12SC;                     // 开始转换
    LcdReset();                               //复位1602液晶
    DispNChar(2,0,12,tishi);                  //显示提示信息
    Disp1Char(11,1,'P');                      //显示浓度单位 
    Disp1Char(12,1,'P');                      //显示浓度单位
    Disp1Char(13,1,'M');                      //显示浓度单位
    _EINT();
    while(1)
     {
      LPM1;
     }
   
   
 }
/*******************************************
函数名称:PutSting
功    能:向PC机发送字符串
参    数:ptr--指向发送字符串的指针
返回值  :无
********************************************/
void PutString(uchar *ptr)
{
      while(*ptr != '\0')
      {
            while (!(IFG1 & UTXIFG0));               
            TXBUF0 = *ptr++;         
      }
      while (!(IFG1 & UTXIFG0));
      TXBUF0 = '\n';
}
/*******************************************
函数名称:PutChar
功    能:向PC机发送一个字符对应的ASCII码
参    数:
返回值  :无
********************************************/
void PutChar(uchar x )
{
          
          while (!(IFG1 & UTXIFG0));
          TXBUF0 =x;
          delay_ms(200);
          //IFG1&=0x00;//清除中断标志位
 
}
/*******************************************
函数名称:UART0_RXISR
功    能:UART0的接收中断服务函数
参    数:无
返回值  :无
********************************************/

#pragma vector = UART0RX_VECTOR                    //UART0的接受中断函数
__interrupt void UART0_RXISR(void)
{    
  

      while (!(IFG1 & URXIFG0));    //等待接收到字符
          RecBuf[Rindex++] = RXBUF0;   //将接收到的数据存放到缓存中                                              
          Disp1Char(pX++,pY,RecBuf[Rindex++]);
         //IFG1=0;//清除中断标志位
            if(pX == 16)
            {
                pX  = 0;   //x--位置的列坐标
                               //y--位置的行坐标
                pY ^= 1;
            }
            delay_ms(10);
}

/*******************************************
函数名称:ADC12ISR
功    能:ADC中断服务函数,用多次平均的
               计算P6.0口的模拟电压数值
参    数:无      
返回值  :无
********************************************/
#pragma vector=ADC_VECTOR
__interrupt void ADC12ISR (void)
{
 
  static uint index = 0;
  results[index++] = ADC12MEM0;               // Move results
  if(index == Num_of_Results)
  {
        uchar i;
        unsigned long sum = 0;
      
        index = 0;
        for(i = 0; i < Num_of_Results; i++)
        {
            sum += results[i];
        }
        sum >>= 5;                         

        Trans_val(sum);
  }
}

/*******************************************
函数名称:Trans_val
功    能:将16进制ADC转换数据变换成三位10进制
                真实的模拟电压数据,并在液晶上显示   
返回值  :无
********************************************/
void Trans_val(uint Hex_Val)
{
    unsigned long caltmp;
    uint Curr_Volt;
    uchar t1,i,j;
    uchar ptr[4];
    caltmp = Hex_Val;
    caltmp = (caltmp << 5) + Hex_Val;           //caltmp = Hex_Val * 33
    caltmp = (caltmp << 3) + (caltmp << 1);     //caltmp = caltmp * 10
    Curr_Volt = caltmp >> 12;                   //Curr_Volt = caltmp / 2^n
    ptr[0] = Curr_Volt / 100;                   //Hex->Dec变换
    t1 = Curr_Volt - (ptr[0] * 100);
    ptr[2] = t1 / 10;
    ptr[3] = t1 - (ptr[2] * 10);
    ptr[1] = 10;                                //shuzi表中第10位对应符号"."
    //在液晶上显示变换后的结果
    for(j=0;j<8;j++)
     { 
    for(i = 0;i < 4;i++)
     {
       Disp1Char((6 + i),1,shuzi[ptr[i]]);
       PutChar(shuzi[ptr[i]]);
       if(ptr[0]>=2&&ptr[2]==0)
        {
         P6OUT=~P6OUT;
        }
     }
     while (!(IFG1 & UTXIFG0));
      TXBUF0 = '\t';             //回车符隔开
     }
    while (!(IFG1 & UTXIFG0));
      TXBUF0 = '\n';           //每8个数据发送完后,换行操作
}

我不知道接收中断函数那样写行不? 我当初以为是不是没有清楚接收中断的标志位IFG1,但是当清除后还是不行,后来一想接收中断又不是多源中断(不像P1口的多源中断),所以不存在清除标志位呀,所以郁闷了~~~~~~              请高手指点。。。。。。

  • 你的代码既然已经用中断函数来处理UART的接收,那就不需要手动在对URXIFG做操作了,430会自动判断URXIFG置位并清零。而你手动清除了IFG0,可能还会对UART的发送产生影响。

    将while (!(IFG1 & URXIFG0));    //等待接收到字符去掉再试试