This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无线通讯之前一步,UART的中断问题



正在做一个无线通讯,外接的是APC240CF的无线通讯模块,设置P2.4输出和P2.5输入,准备在USART0的通讯基础上实现,485通讯我已经实现了,经过删减后,但是我发现我的这个程序无法进入通讯中断。其次我把whil(1)和中断标志位进入判定语句receive_flag==1:删除后,427芯片TXD脚可以保持一直发送固定的信号,但是RXD脚也受到了影响,也一致产生固定的信号,起波长与TXD的波几乎一致,只是开头和结尾为1,中间为0。当不删除的时候(即如下程序)示波器可以观察,不过这样用示波器观察在进入mian.c之后要执行WMSendRDData(ComBuf);的时候与我预计的没什么问题,毕竟度只是初始化,但是一执行WMSendRDData(ComBuf);语句请教下我这边是出现了什么问题了?附程序和头文件
主程序 main.c
#include  <msp430x42x.h>
#include  "main.h"  
uchar8 ComBuf[COMBUFLEN];
uchar8 BufNum=0;
uint32 FV=5432;       // 流速 Flow Velocity   
uint32 FL=1111;   // 流量   
int receive_flag=0;
uchar8 WMAddress[7]={1,2,3,4,5,6,7};
void InitUART0(void) //波特率初始化
{
// case 1200:
    UTCTL0 = SSEL0;       // UCLK = ACLK
    UBR00 = 0x1b;         // 32768/1200 = 27.307
    UBR10 = 0x00;                        
    UMCTL0 = 0x11;        //调整字节UMCTL0中1的个数为0.307*8=2.45≈2,均匀分布1得到0x11
}
void BasicTimer_Init (void)                                // BasicTimer On
{
    BTCTL |= BTDIV + BT_fCLK2_DIV16;            // ACLK/(256*16)
    IE2   |= BTIE;                              // Enable BT interrupt
}

void DisableWDT(void)//About WDT   关闭看门狗  
{
  WDTCTL = WDTPW + WDTHOLD;                   // Stop WDT  
}
void DCO_Init(void)//DCO初始化
{
  uint16 i;
  
  FLL_CTL0    = XCAP18PF + DCOPLUS;           // Configure MCLK
  SCFQCTL     = 60;                               
  SCFI0       = FLLD_2;                                    // SMCLK = MCLK = 32.768*(60+1)*2 = 399.77K
  SCFI1       = 0;      
  
  do {
    IFG1 &= ~OFIFG;                         // Clear oscillator fault flag
    for (i = 5000; i; i--);                // Delay
  } while(IFG1 & OFIFG);                      // Test osc fault flag  
}

//串口初始化
void Uart0_Init(void)  
{
  P2SEL|=BIT4+BIT5;
  P2DIR|=BIT4;
  P2DIR&=~BIT5;
  U0CTL |= SWRST;                //控制寄存器位
  U0CTL &= ~(SYNC + MM);
  UCTL0  |= CHAR + PEV + PENA;                // 8-bit character
  InitUART0();
  ME1    |= UTXE0 + URXE0;                    // Enable USART0 TXD/RXD
  UCTL0  &=~SWRST;                            // Initialize USART state machine

  IE1    |= URXIE0;                           // Enable USART0 RX interrupt   
  IE1   &=~ UTXIE0;              //发送中断关闭;
  IFG1   = 0X00;                 //中断标志位清零
}

//发送一个字节
void TxdOneByte(uchar8 ch)
{
  while(!(UTCTL0 & TXEPT));
  TXBUF0 = ch;
}

//发送一个缓冲帧
void TxdBuf (uchar8 buf[],uchar8 len)
{
  int i;
  for(i = 0; i < len; i++) {
    TxdOneByte(buf[i]);
  }
}
void LToOctal(unsigned char *ptr, unsigned long mun)
{
  int i=4;
  for(;i>=0;i--)
  {
    ptr[i]=mun%10;
    mun=mun/10;
  }
}
void delay(int ms)
{
  int sub=200;
  for(;ms>=0;ms--)
  sub--;
}
///////////////////////////////////////////////////////////////////////   
#pragma vector =UART0RX_VECTOR
__interrupt void USART0_RX (void)
{
delay(100);
  _DINT();
  receive_flag=1;
  ComBuf[BufNum++] = RXBUF0;
  if(BufNum == COMBUFLEN) //防止溢出
    BufNum = 0;     
    _EINT();
}
//水表接收到读操作后返回的响应数据处理
void WMSendRDData(uchar8 pdata[])        //pdata为串口接收到的数据,RtnRslt为返回的帧起始地址
{
  uchar8 rtnrslt[60];
  uchar8 i=0,check=0;
  
  for(i=0;i<4;i++)
    rtnrslt[i] = 0XFE;//COMLEADER;
  rtnrslt[i++] = 0X68;//COMHEAD;
  rtnrslt[i++] = 0X16;//COMTYPE;
  rtnrslt[i++] = WMAddress[0];
  rtnrslt[i++] = WMAddress[1];
  rtnrslt[i++] = WMAddress[2];
  rtnrslt[i++] = WMAddress[3];
  rtnrslt[i++] = WMAddress[4];
  rtnrslt[i++] = WMAddress[5];
  rtnrslt[i++] = WMAddress[6];
  rtnrslt[i++] = pdata[9]+0x80;        //返回的应答命令为原命令再加0x80
  rtnrslt[i++] = 0x16;//LENREADDATA;
  rtnrslt[i++] = pdata[11]; //DI0
  rtnrslt[i++] = pdata[12]; //DI1
  rtnrslt[i++] = 0;   //SER
      LToOctal(&rtnrslt[50],FL);   //当前累积流量,定点数,两位小数
      rtnrslt[i++] = rtnrslt[53];
      rtnrslt[i++] = rtnrslt[52];
      rtnrslt[i++] = rtnrslt[51];
      rtnrslt[i++] = rtnrslt[50];
      rtnrslt[i++] = 0x2C;          //单位  m3
      
      LToOctal(&rtnrslt[50],FV);   //瞬时流量,定点数,4位小数
      rtnrslt[i++] = rtnrslt[53];
      rtnrslt[i++] = rtnrslt[52];
      rtnrslt[i++] = rtnrslt[51];
      rtnrslt[i++] = rtnrslt[50];
      rtnrslt[i++] = 0x35;          //单位  m3/h

//      rtnrslt[i++] = Data8ToBCD(30);   //实时时间,sec
//      rtnrslt[i++] = Data8ToBCD(WorkTime.min/480);   //实时时间,min
//      rtnrslt[i++] = Data8ToBCD(WorkTime.hour);     //实时时间,hour
//      rtnrslt[i++] = Data8ToBCD(WorkTime.day);      //实时时间,day,
//      rtnrslt[i++] = Data8ToBCD(WorkTime.month);    //实时时间,月
//      rtnrslt[i++] = Data8ToBCD(WorkTime.year);     //实时时间,年低八位
//      rtnrslt[i++] = 0x20;            //实时时间,年高八位

      rtnrslt[i++] = 0;            //水表状态ST1 用户自定义
      
      rtnrslt[59] = i;
      for(i=4;i<(rtnrslt[59]);i++)//校验计算
      {
        check += rtnrslt[i];
      }
      i = rtnrslt[59];
        rtnrslt[i++] = check;
  rtnrslt[i++] = 0X16;//COMREAR;        //帧结束
  TxdBuf(rtnrslt,i);
}
void main(void)   //主程序
{
  DisableWDT();  //禁止看门狗,方便系统初始化
  DCO_Init();
  BasicTimer_Init();
  Uart0_Init();

   while(1)
  {
if (receive_flag==1)
{
  WMSendRDData(ComBuf);
  receive_flag=0;
}
  Delay_ZZG(200);
  }

}


void Delay_ZZG(unsigned int ms)   
{                              
unsigned int i,j;
for( i=0;i<ms;i++)
for(j=0;j<2000;j++);        //8MHz晶振时
}








//将无符号8位数据转换成压缩BCD码
uchar8 Data8ToBCD(uchar8 dat)
{
  uchar8 bcd=0;
  
  if(dat > 99)
    return 0;
  
  while(dat > 9)
  {
    dat -= 10;
    bcd++;
  }
  bcd <<= 4;
  bcd += dat;
   
  return bcd;  
}

const uchar8 BCD_DA_Table[10]={0,6,12,18,24,30,36,42,48,54};//BCD码的十进制调整DA的参数表

//将压缩BCD码转换成无符号8位数
uchar8 BCDToData8(uchar8 bcd)
{
  return(bcd - BCD_DA_Table[bcd>>4]);
}
头文件main.h
#ifndef _MAIN_H_
#define _MAIN_H_
//#include  <string.h>

//////////////////////////////////////////////////////
typedef unsigned char uchar8;
typedef unsigned int uint16;           
typedef unsigned long uint32;
typedef unsigned long long uint64;

#define COMBUFLEN 120
#define ComSendBuf (ComBuf+80)    //接收缓冲大小,后40字节并共用于半双工通信时的发送
//#define  COMREAR 16
//#define  COMLEADER 16

//函数外部声明
extern unsigned char ComBuf[COMBUFLEN];

extern void Uart0_Init (void);
extern void TxdOneByte(uchar8 ch);
extern void TxdBuf (unsigned char buf[],unsigned char len);


//extern unsigned char WMRcvDataProcess(unsigned char pdata[], unsigned char rtnrslt[]);//水表接收到的串口帧数据预处理,进行帧判断和错误处理
extern void WMSendRDData(unsigned char pdata[]);        //水表接收到读操作后返回的响应数据处理//pdata为串口接收到的数据,RtnRslt为返回的帧起始地址

extern void InitUART0(void);
extern void  LToOctal(unsigned char *ptr, unsigned long mun);// rljasm.s43

extern unsigned char Data8ToBCD(unsigned char dat);// rljasm.s43 //将数据转换成压缩BCD码
extern unsigned char BCDToData8(unsigned char bcd);//将压缩BCD码转换成无符号8位数

extern void BasicTimer_Init (void);  

extern  void Delay_ZZG(unsigned int ms);


#endif