Other Parts Discussed in Thread: MSP430F6720
最近在做一个项目,用到了MSP430F6720,之前做了一块测试板,程序都写好了,测试没有问题。于是我将板子重新画了一下,结果XT1就不起震了。之前的板子上有些引脚(AUXVCC1、AUXVCC2、AUXVCC3、LCDAP、VDSYS、DVSYS)没有按照数据手册上要求的处理,而在新做的板子上完全依照数据手册上处理的,结果反而不能用了。不过好像不是这些管脚的问题,因为我通过割线的方法也试过将其改回到原来的接线方式,结果问题依旧。XT1我采用的32768HZ晶振,我可以确定是XT1的问题,首先在晶振上测不到波形(在之前的板子上可以),然后我在程序上将时钟源改为REFO后其他模块(比如串口)就正常工作了。还有一个奇怪的问题,XT1的错误标志并没有置位,反而DCO的错误标志置位了,但是我用的FLL可以正常工作。
我用万用表测量的AVCC的DVCC都是3.3V,该接地的地方全都接地。XIN和XOUT也都连接晶振,我想问除了XIN与XOUT外,XT1还与其他哪个管脚有关系吗