This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5739的USCI通道A中的IrDA和UART功能可以同时使用么?



MSP430新手~~

想利用MSP430单片机进行数据采集与红外的数据发送,数据有两路,分别为SPI和UART接口的,需要各占用一个接口,对数据处理后通过红外接口进行数据发送,实现SIR的115.2kbps的数据传输,不知道能不能利用MSP430F5739实现?

看手册说明是MSP430F5739的USCI有两个通道A、B,Ch A: UART/LIN/IrDA/SPI,Ch B: I2C/SPI ,CHA有2个,就是不知道这个CHA的2路(IrDA)和CHB的spi能不能同时使用,谢谢!

新手望不吝赐教!~