This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTC_C 系統掉電保持運作問題

Other Parts Discussed in Thread: MSP430F6720

您好~我使用MSP430F6720

電路:AUXVCC1 ,AUXVCC2 接地,AUXVCC3 接電池

目的:  為了確保斷電後RTC_C 能透過電池能保持運作就好,其他周邊電源不須保持。

目前在CODE 的部分 先進行AUX 設定

因不須備用電源 關閉了AUX1 與 AUX2

AUXCTL1 |= AUX1MD|AUX2MD; // AUX2MD=1
AUXCTL1 &= ~(AUX1OK|AUX2OK); // AUX2OK=0

在 RTC init 時 運行

if (SYSRSTIV == SYSRSTIV_LPM5WU)
{
     // When woken up from LPM3.5, reinit since LPMx.5 will cause a BOR.
     PMMCTL0_H = PMMPW_H; // open PMM
     PM5CTL0 &= ~LOCKIO; // Clear LOCKBAK and enable ports
     PMMCTL0_H = 0x00; // close PMM

// Reconfigure RTC to read RTC registers
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL0_H))) = RTCKEY_H;
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) |= RTCHOLD;
(*((volatile uint16_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) &= ~(RTCBCD);
(*((volatile uint16_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) |= RTC_C_FORMAT_BCD;
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) &= ~(RTCHOLD);
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL0_H)))= 0x00;
}else{
// Reconfigure RTC to read RTC registers
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL0_H))) = RTCKEY_H;
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) |= RTCHOLD;
(*((volatile uint16_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) &= ~(RTCBCD);
(*((volatile uint16_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) |= RTC_C_FORMAT_BCD;
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL13_L))) &= ~(RTCHOLD);
(*((volatile uint8_t*)((uint16_t)RTC_C_BASE + OFS_RTCCTL0_H)))= 0x00;
}

// GPIO Port Configuration for lowest power configuration
P1OUT = 0x00;P2OUT = 0x00;P3OUT = 0x00;P4OUT = 0x00;P5OUT = 0x00;P6OUT = 0x00;
P7OUT = 0x00;P8OUT = 0x00;P9OUT = 0x00;PJOUT = 0x00;
P1DIR = 0xFF;P2DIR = 0xFF;P3DIR = 0xFF;P4DIR = 0xFF;P5DIR = 0xFF;P6DIR = 0xFF;
P7DIR = 0xFF;P8DIR = 0xFF;P9DIR = 0xFF;PJDIR = 0xFF;
RTC_C_setCalendarEvent(RTC_C_BASE,RTC_C_TIME_EVENT_INTERRUPT);
RTC_C_setCalendarEvent(RTC_C_BASE,RTC_C_CALENDAREVENT_MINUTECHANGE);
RTC_C_enableInterrupt(RTC_C_BASE,RTCRDYIE + RTCTEVIE );
//Start RTC Clock
RTC_C_startClock(RTC_C_BASE);

但還是無法達到我所需要的目的

目的:  為了確保斷電後RTC_C 能透過電池能保持運作就好,其他周邊電源不須保持。

請教各位先進~~