This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AD在无输入的情况下跳动!!

Other Parts Discussed in Thread: MSP430F5418A

    如题:MCU为MSP430F5418A,采用外部基准3.3V,输入为8路滑动变阻器(可与AD连接分离),现在存在的问题:

1、将滑动变阻器与MCU分离,AD在无输入的情况下,有数据在不停跳动,大概100mV左右。

采取过的措施:a、在AD输入通过200K电阻接地;b、AD串联一个电阻100欧,并联一个102的电容(手册中推荐的接口电路)。

通过措施a,跳动的频率慢了,但是还是会跳动;通过措施b没有任何改善。

有人说外部基准不稳定,我分别把AD输入接AD基准和地,均无数据跳变。说明基准是稳定的,地上也无干扰。

2、接上8路滑动变阻器,其中有一路信号,在没有改变滑动变阻器的情况下,会有跳动。

求教过各位大神,这种现象要怎么解决??