之前是使用msp-gang programmer对430G2433进行烧录一台烧一个,电压选择的是3.3V,后来听说可以使用这个烧录器一拖八,然后试了下,电压3.3V的时候只能烧录一个,然后我将电压调到3.0V的时候,就可以同时烧录3个了。小弟菜鸟一个,那位大神能够帮我解惑一下,这样会不会有什么问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前是使用msp-gang programmer对430G2433进行烧录一台烧一个,电压选择的是3.3V,后来听说可以使用这个烧录器一拖八,然后试了下,电压3.3V的时候只能烧录一个,然后我将电压调到3.0V的时候,就可以同时烧录3个了。小弟菜鸟一个,那位大神能够帮我解惑一下,这样会不会有什么问题?
关于MSP-GANG的使用,您可以参考用户手册 http://www.ti.com.cn/cn/lit/ug/slau358g/slau358g.pdf
需要注意
1 配置参数和引脚连接要正确
2 当同时烧写8片时,不能使用USB供电方式,必须采用外部供电方式。因为USB能承载的电流太小。
3 烧写信号线不要太长