Other Parts Discussed in Thread: MSP430FR5994
想请问下各位
看MSP430选型手册FRAM系列MCU中说到“Configurable as program or data memor”,是不是可以将部分FRAM分配给SRAM?如果可以的话怎么实现?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FR5994
想请问下各位
看MSP430选型手册FRAM系列MCU中说到“Configurable as program or data memor”,是不是可以将部分FRAM分配给SRAM?如果可以的话怎么实现?
谢谢!
您好!
我做的项目目前遇到的问题是想把FRAM当做EEPROM来使用,我尝试直接给FRAM写数据,掉电后数据还是会丢失,我想问一下,能否有相关的FRAM当做EEPROM来使用?项目非常着急,期待各位的回答,非常感谢!
另外我想知道FRAM当做EEPROM使用是FR系列的亮点,为什么没有相关的示例呢,很是困惑!
你好, FRAM 读写都有范例代码的。
掉电保存
#include <msp430.h>
void FRAMWrite(void);
unsigned char count = 0;
unsigned long *FRAM_write_ptr;
unsigned long data;
#define FRAM_TEST_START 0x1800
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state
P1DIR |= BIT0; // Set P1.0 to output directionOUT
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
data = 0x11111111; // Initialize dummy data
while(1)
{
data += 0x00010001;
FRAM_write_ptr = (unsigned long *)FRAM_TEST_START;
FRAMWrite();
count++;
if (count > 100)
{
P1OUT ^= 0x01; // Toggle LED to show 512K bytes
count = 0; // ..have been written
data = 0x11111111;
}
}
}
void FRAMWrite (void)
{
unsigned int i=0;
SYSCFG0 &= ~DFWP;
for (i = 0; i < 128; i++)
{
*FRAM_write_ptr++ = data;
}
SYSCFG0 |= DFWP;
}您好:
感谢您的提示,这个代码之前我测试不行,昨天测试就可以了,
我想请教一下,我需要存放变量的地址是需要自己在FRAM中划分出一块专门来存放变量,还是说我随便都可以定义一个起始地址开始存放,如果这样可以的话,烧写代码或者代码运行的过程中,这些地址的内容会不会被误操作,期待您的回复,谢谢!
您说的配置,能说的具体一点吗,我应该怎么设置就是传统的FLASH,怎么做是SRAM,又怎么做是EEPROM?这个感觉太模糊了,
还是说FRAM本身就具备这三种特性,只是看我自己使用他的什么特性?期待您的解释,谢谢!
用户数据一般存放在数据区,这样就可以避免程序代码被改掉。
有一些FRAM的产品是带MPU的,建议看一下数据手册和用户手册。
m 说:MSP4330FR5994,不过我没有加
SYSCFG0 &= ~DFWP 数据也能写进去,不知道为什么
//******************************************************************************
// MSP430FR5x9x Demo - Long word writes to FRAM
//
// Description: Use long word write to write to 512 byte blocks of FRAM.
// Toggle LED after every 100 writes.
// NOTE: Running this example for extended periods will impact the FRAM
// endurance. MPU is also enabled by default in CCS.
// MCLK = SMCLK = default DCO
//
// MSP430FR5994
// ---------------
// /|\| |
// | | |
// --|RST |
// | |
// | |
// | P1.0 |---> LED
//
// William Goh
// Texas Instruments Inc.
// October 2015
// Built with IAR Embedded Workbench V6.30 & Code Composer Studio V6.1
//******************************************************************************
#include <msp430.h>
#define WRITE_SIZE 128
void FRAMWrite(void);
unsigned char count = 0;
unsigned long data;
#if defined(__TI_COMPILER_VERSION__)
#pragma PERSISTENT(FRAM_write)
unsigned long FRAM_write[WRITE_SIZE] = {0};
#elif defined(__IAR_SYSTEMS_ICC__)
__persistent unsigned long FRAM_write[WRITE_SIZE] = {0};
#else
#error Compiler not supported!
#endif
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure GPIO
P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state
P1DIR |= BIT0; // Set P1.0 to output direction
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Initialize dummy data
data = 0x00010001;
while(1)
{
data += 0x00010001;
FRAMWrite();
count++;
if (count > 100)
{
P1OUT ^= 0x01; // Toggle LED to show 512K bytes
count = 0; // ..have been written
data = 0x00010001;
}
}
}
void FRAMWrite(void)
{
unsigned int i = 0;
for (i = 0; i < 128; i++)
{
FRAM_write[i] = data;
}
}#pragma PERSISTENT(FRAM_write) unsigned long FRAM_write[WRITE_SIZE] = {0};program will not fit into available memory. placement with alignment fails for section "RW_IPE" size 0x107fe lnk_msp430fr5994.cmd /OBEM_MSP430FR5994 line 147 C/C++ Problem
应该如何处理,修改 .com文件吗?