This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:MSP430F1490写入nmi测试后,不能使用BSL下载,应该如何解决??????



由于没有下载器,因此一直使用BSL下载方式进行430的学习。

测试NMI程序,采用淘宝的电路板,和官方的NMI程序,如下:

#include  <msp430x14x.h>

void main(void)
{
  WDTCTL = WDTPW + WDTHOLD + WDTNMI + WDTNMIES;  // WDT off NMI hi/lo
  P1DIR |= 0x01;                            // Set P1.0 to output direction
  P1OUT &= ~0x01;                           // Clear P1.0 LED off
  IE1 |= NMIIE;                             // Enable NMI

  _BIS_SR(LPM0_bits);                       // Enter LPM0
}

#pragma vector=NMI_VECTOR
__interrupt void nmi_ (void)
{
  volatile unsigned int i;
  P1OUT |= 0x01;                            // Set P1.0 LED on
  for (i = 20000; i > 0; i--);              // Delay
  P1OUT &= ~0x01;                           // Clear P1.0 LED off
  IFG1 &= ~NMIIFG;                          // Reclear NMI flag in case bounce

  IE1 |= NMIIE;                             // Enable NMI
}

结果编程下载完后,就不能再次进行BSL下载测试了,BSL软件显示错误如下:

15:15:02  Erase failed. Synchronization error.

感觉应该是NMI程序使得RESET引脚不能复位,因此不能同步。

请问还没有办法擦除芯片内的程序,或者还是说开发板已经变砖了?

  • 把和复位引脚相连的上拉电阻和电容焊下来,然后在复位引脚上接一个1k的下拉电阻(注意是下拉),这样单片机在上电以后由于复位引脚为低,从而不工作,(复位引脚此时还是默认的复位功能),这时候再下程序,就能成功了。要多试几次~~~

  • 我只有一个BSL下载,也就是USB下载线,按照你的说法,试了十多次,都是显示的FLASH擦除失败,我就一直用BSL进行擦除,也是不行的。

    还是说你这方法只能在JTAG下才能使用?