1602的RS接P2.0,RW接P2.1,E接P2.2
7~14的8个引脚接MSP430的P1.0~P1.7,其余按照1602引脚要求连接。
#include<msp430g2553.h>
#define uchar unsigned char
#define uint unsigned int
#define P20 0
#define P21 1
#define P22 2
#define RS_CLRP2OUT &= ~(1 << P20) //RS置低
#define RS_SETP2OUT |= (1 << P20) //RS置高
#define RW_CLRP2OUT &= ~(1 << P21) //RW置低
#define RW_SETP2OUT |= (1 << P21) //RW置高
#define EN_CLRP2OUT &= ~(1 << P22) //E置低
#define EN_SETP2OUT |= (1 << P22) //E置高
uchar num;
int ADC_CHO;
int c;
int data;
unsigned char x;
unsigned char y;
void delay(uint z)
{
uint x,y;
for(x=z;x>0;x--)
for(y=110;y>0;y--);
}
void write_com(uchar com) //输入数据
{
RS_CLR; //RS置低 输入指令
P1OUT=com;
delay(5);
EN_SET;
delay(5);
EN_CLR; //E置低 1->0 执行指令
}
void write_data(uchar data) //输出数据
{
RS_SET; //RS置高 RS=1输出数据
P1OUT=data;
delay(5);
EN_SET;
delay(5);
EN_CLR; //E置低 1->0 执行指令
}
void init() //1602初始化,请参考1602的资料
{
EN_CLR;
write_com(0x38); //设置16*2显示,5*7点阵,8位数据接口
write_com(0x0e); //光标不显示
write_com(0x06); //写入新数据后光标右移,显示频不移动
write_com(0x01); //0000000001 清屏
write_com(0x80); //修改指针的位置
}
void display_xy(unsigned char x,unsigned char y)
{
if(y==0x01)
{
x = x + 0x40 + 0x80; }
else
{
x = x+0x80; //数据指针设置 80H+地址码 (0-27H,40H-67H)
}
write_com(x);
}
void Disp1Char(uchar x,uchar y,uchar data)
{
display_xy(x,y);
write_data(data); ////输出数据
}
void Disp_float(float f_data)
{
unsigned char lcd_table[3];
int aa;
aa=f_data;
lcd_table[0]= aa/100;
lcd_table[1]= aa%100/10;
lcd_table[2]=aa%10;
Disp1Char(5,0,(lcd_table[0]+0x30)); //显示整数部分的十位数 0x30的原因CGROM和CGRAM与字符的对应关系
Disp1Char(6,0,(lcd_table[1]+0x30));//显示小数部分的个位
Disp1Char(7,0,(0x2e)); //显示小数点"." 小数点对应00101110
Disp1Char(8,0,(lcd_table[2]+0x30)); //显示小数部分的十分位
//加上0x30以便直接得到相应的ASCII码去显示
}
void main()
{
WDTCTL = WDTPW + WDTHOLD;
P2DIR = 0XFF;
P1DIR = 0XFF; //输出all
P1OUT = 0;
RW_CLR; //写数据指令
init();
ADC10CTL1 |= CONSEQ_2; //单通道多次转换模式
ADC10CTL0 |= SREF_1+REFON;//REFON=1选择内部参考源1.5,VR+=VREF+and VR-=VSS,打开基准源
ADC10CTL0 |= ADC10SHT_3+MSC;//过采样率设置为64个采样周期,打开AD转换,MSC多次采样
ADC10CTL1 |= ADC10SSEL_3+SHS_0;//ACLK2分频为采样时钟,用ADC10SC触发采集
ADC10CTL1 |= INCH_10;//选择通道10
ADC10CTL0 |= ADC10ON;//开启ADC10
while(1)
{
delay(1000);
ADC10CTL0 |= ENC + ADC10SC; // 开始转换 ENC为转换使能位,ADC10SC转换控制位
while((ADC10CTL0 & ADC10IFG)==0);//等待ADC10IFG标志位变高(转换完成)
ADC_CHO= ADC10MEM;//读取采样结果
data =(ADC_CHO-746)/(0.000335*678)+286;//计算温度值
c=data;
if(c>150)
{P2DIR |= BIT3;
P2OUT=0x00;
delay(2000); }
Disp_float(c); //显示结果
delay(2000);
}
}