实验中需要采集5V电压,因为高于430 3.3V的工作电压,如果采用内部ADC进行采集,应该如何实现?
430的内部ADC采用外部输入参考电压5V是否可行?
另外也有提到用电阻分压至430允许电压范围内的,电压阻值是否有要求?
请专家指点,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实验中需要采集5V电压,因为高于430 3.3V的工作电压,如果采用内部ADC进行采集,应该如何实现?
430的内部ADC采用外部输入参考电压5V是否可行?
另外也有提到用电阻分压至430允许电压范围内的,电压阻值是否有要求?
请专家指点,谢谢!
如果AD的输入阻抗足够高简单地用两个电阻分压。
如果AD输入阻抗比较低,两个电阻分压后加跟随器。
那么对于430的SAR型ADC ,这种ADC内阻都很大,一般500K以上。即使阻抗小的ADC,阻抗也是固定的。所以即使只要被测源内阻稳定,只是相当于电阻分压,可以被校正。
你好 我看了你在这片帖子的回复,我想问一下,电压跟随器是只有一个增大输入阻抗的作用吗,还有一点就是 电压跟随器是需要自己搭建的电路吗 还是是有这样成型的芯片的啊