This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在使用A0通道检测电压的变化,直接用可调电源给0~3.3V 到P60,检测出0~4096数字量基本和输入电压成线性关系。 然后用200HZ的PWM信号(占空比0~100%可调),经过三阶RC(20K+0.47UF),输入到P60,
得到的数字量和占空比的线性关系变得很差,请问ADC前端输入电路有什么需要注意的?我的目的就是检测PWM信号的占空比,不需要很精确但要成线性关系(MCU定时器资源全部被占用了,无法使用定时器捕获)