This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题1:MSP430F4250定时器A能否同时计时两路,需求是一个15分钟定时自动关机,一个是中断按键定时器延时!两个定时互不影响!
问题2:MSP430FG479的LCD模块,能否选择性的使用S段,比如我不使用S0-S3,这四个管脚作为普通IO使用(需使用管脚的中断功能),我将S4-S19选通作为LCD的段!用来显示字符!
问题3:MSP430F4250的LCD的COM口的四个管脚是否可以交换连接,比如MCU的COM0接屏幕的COM3;MCU的COM1接屏幕的COM2,依次这样连接,是否可以,如果可以,会出现什么样的效果!比如各个地址对应的段变化了!
问题4:MSP430F4250使用P1口的中断按键进入LPM4,也用P1按键退出LPM4;需求是,P1.2为HOLD功能,P1.3为屏幕背光,P1.4为低功耗开光,要求按键进入低功耗模式4后,只能由P1.4的开关唤醒,不能由P1.2和P1.3唤醒!
问题5:MSP430FG479的SVS功能,如果使用外部输入源的话,是不是就是只能和基准电压1.2V比较,不能像供电电源那样和其他多个可选择值比较!
以上4个问题,求大虾指教!非常感谢!!!!!