在使用430mcu时,发现了两个问题:
1.在使用随机数rand()中,使用了rand()&0xff,会造成重启,最后就改成rand()%256;问题原因还没找出来。
2.在使用按键中断时,配置了上边沿触发,但是测试发现只要触发了两次,应该是上下边沿都触发了,不知道为什么,已经去抖了,不应该是这个问题。
请大家帮忙分析下以上两个问题,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用430mcu时,发现了两个问题:
1.在使用随机数rand()中,使用了rand()&0xff,会造成重启,最后就改成rand()%256;问题原因还没找出来。
2.在使用按键中断时,配置了上边沿触发,但是测试发现只要触发了两次,应该是上下边沿都触发了,不知道为什么,已经去抖了,不应该是这个问题。
请大家帮忙分析下以上两个问题,谢谢!
1.对于随机数代码主要是我要实现定时器,如下:
CCR0 = (SYS_CLK_32k>>2)+(rand()%256);// 不会重启;
CCR0 = (SYS_CLK_32k>>2)+(rand&0xFF);// 会重启,不是必然的;
2.按键中断配置如下:
gpio_int_enable(PORT1, (KEY0 | KEY1), INT_RISE_EDGE); //上升沿触发;看了文档,触发方式只能二选一,不知道我的为什么会触发两次?
实现如下:
void gpio_int_enable(uint8 port, uint8 pin, uint8 int_type)
{
if (port == PORT1)
{
P1IE |= pin; // KEY引脚中断使能
if (int_type == INT_FALL_EDGE)
P1IES |= pin; // 下降沿中断
else
P1IES &= ~pin; // 上升沿中断
P1IFG &= ~pin; // 清除中断标志
}
else if (port == PORT2)
{
P2IE |= pin; // KEY引脚中断使能
if (int_type == INT_FALL_EDGE)
P2IES |= pin; // 下降沿中断
else
P2IES &= ~pin; // 上升沿中断
P2IFG &= ~pin; // 清除中断标志
}
}