This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC430F5137的温度问题

Other Parts Discussed in Thread: CC430F5137

2个问题,希望客服同志能够给予比较详细的解答,谢谢。

1、CC430F5137 的存储温度我现在看到2个版本,一个是-55℃~105℃,还有一个是-55℃~150℃,到底以哪个为准?

2、CC430F5137的工作温度是-40~85℃,最高节温是95℃,如果我的IC处于LPM3或LPM4模式的情况下,能不能抗住110℃的温度?如果不行,有没有满足要求的替代品?

  • 不是TI的客服,我说说个人的建议.

    CC430这个系列的工作温度目前是-40~85℃。如果用在110℃是有风险的,真要这么用的话建议做下模拟试验。

    不过,msp430系列的单片机有-40~85℃、-40~105℃,部分型号更有增强型的,可以工作在-40~125℃。

    如果成本可以接受的话,可以使用增强型msp430+外置射频来实现

  • daming,

      根据最新版的datasheet,应该是以150为准。

    我们的芯片推荐工作温度是-40~85度,如果你需要工作在110的话,会出现不可预计的问题,我们不建议也不推荐你用在这个温度范围。

    谢谢