This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS使用问题!!!



CCS版本为5.4.0。使用中遇到这么几个问题
   
     1. 已有一个名为Demo的Project,能够正常打开和编译。将Demo复制一份,命名为Demo1,与Demo存放在同一路径下。

         结果发现“Import CCS Eclipse Project”时,提示“Some projects cannot be imported because they already exist in the workspace”

         无法将其在“Project Explorer”中打开。

     2. 在“TI Resource Explorer”中正常导入一个项目,比如“MSP430F55xx_WDT_01”;

         然后再从“TI Resource Explorer”中将其Delete;

         当我再次想将“MSP430F55xx_WDT_01”这个项目导入到“TI Resource Explorer”中时,提示错误信息如下:

         “Issue that may requir your attention were encountered while creating the project(s)”,

         “Detail”显示为“An Eclipse project already exists at location 'C\.......'”,为什么会这样呢??