This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fatal Error[Pe035]: #error directive: Compiler not recognised



rebuild 工程时,出现:Fatal Error[Pe035]: #error directive: Compiler not recognised

程序:

#ifndef _ISR_COMPAT_H_
#define _ISR_COMPAT_H_

/* Cross compiler interrupt service routine compatibility definitions */
/* This code currently allows for:
MSPGCC - the GNU tools for the MSP430
Quadravox AQ430
IAR Version 1 (old syntax)
IAR Versions 2 and 3 (new syntax)
Rowley Crossworks
Code Composer Essentials

These macros allow us to define interrupt routines for all
compilers with a common syntax:

ISR(<interrupt>, <routine name>)
{
}

e.g.

ISR(ADC12, adc_service_routine)
{
ADC12CTL0 &= ~ENC;
ADC12CTL0 |= ENC;
}
*/
#if defined(__AQCOMPILER__)
/* This is the Quadravox compiler */
#define ISR(a,b) void _INTERRUPT[a##_VECTOR] b(void)
#elif defined(__IAR_SYSTEMS_ICC__) && (((__TID__ >> 8) & 0x7f) == 43) && (__VER__ < 200)
/* This is V1.xx of the IAR compiler. */
#define ISR(a,b) interrupt[a##_VECTOR] void b(void)
#elif defined(__IAR_SYSTEMS_ICC__) && (((__TID__ >> 8) & 0x7f) == 43) && (__VER__ < 600)
/* A tricky #define to stringify _Pragma parameters */
#define __PRAGMA__(x) _Pragma(#x)
/* This is V2.xx, V3.xx, V4.xx, or V5.xx of the IAR compiler. */
#define ISR(a,b) \
__PRAGMA__(vector=a##_VECTOR) \
__interrupt void b(void)
#elif defined(__CROSSWORKS_MSP430)
/* This is the Rowley Crossworks compiler */
#define ISR(a,b) void b __interrupt[a##_VECTOR](void)
#elif defined(__TI_COMPILER_VERSION__)
/* This is the Code Composer Studio compiler. */
/* A tricky #define to stringify _Pragma parameters */
#define __PRAGMA__(x) _Pragma(#x)
#define ISR(a,b) \
__PRAGMA__(vector=a##_VECTOR) \
__interrupt void a##_ISR(void)
#elif defined(__TI_COMPILER_VERSION)
/* This is the Code Composer Essentials compiler. */
#define ISR(a,b) __interrupt void b(void); \
a##_ISR(b) \
__interrupt void b(void)
#elif defined(__GNUC__) && defined(__MSP430__)
/* This is the MSPGCC compiler */
#define ISR(a,b) interrupt(a##_VECTOR) b(void)
#else
#error Compiler not recognised.
#endif

#endif