This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: MacBook无法连接到MSP430G2553

Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP-EXP430G2ET

我购买的单片机型号为MSP430G2553(官网买的正品),在MacBook上的Code Composer Studio 12.4.0软件(官网下载的正品)上运行编写好的代码,代码本身没有问题。将单片机连接到电脑上后,需要将代码烧录到单片机内,结果Code Composer Studio 12.4.0软件弹出如下错误:

MSP430: Error initializing emulator: No USB FET was found

可以看出来电脑没有识别出单片机。我的MacBook型号是MacBook Air,Apple M1芯片,2020年款,系统是macOS Ventura 13.6。之后我检查了与单片机相连接的拓展坞和数据线,均没有问题。将单片机与电脑连接后,单片机的LED0灯和LED1灯会亮起,LED0亮绿灯,LED1亮红灯,LED2会闪烁,但电脑上没有任何通知显示已经识别出单片机。我后来怀疑是电脑的驱动问题,导致识别不出单片机。之后询问了我认识的相关技术人员,他告诉我在Windows系统上需要找到如下路径

然后将该路径下的四个文件用其他四个同名文件替换掉(同名文件如下),他跟我解释说CCS软件虽然自带驱动程序文件使电脑可以识别出单片机,但不知什么原因识别不出MSP430G2553型号的单片机,所以需要修改CCS软件的驱动程序文件,那四个同名文件即是修改后的驱动程序文件。但此方法只适用于Windows系统,macOS系统找不到CCS软件的驱动程序文件,找到了也不知道怎么修改。且我也不确定他向我提供的解决方法是否正确,还是因为别的什么原因导致我的电脑识别不到单片机。

驱动.zip