This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
guide里写:
111 Reset/Set
The output is reset when the timer counts to the TACCRx value. It is set when the timer
counts to the TACCR0 value.
那么对于需要调节占空比的PWM,当调节到TACCRx=TACCR0时到底是什么情况呢?100%占空比能实现么?
另外,内部的EQUx的时序是怎样的?
产生100%占空比要看是哪种模式:
1、上升模式:TACCRx >= TACCR0+1
2、上升下降模式:TACCRx >= TACCR0
EQUx 是哪个由比较值大小来决定产生的先后
还是不太明白
那个框图不用贴了吧?
输出模式 7 PWM 复位/置位模式:
输出电平在 TAR 的值等于 TACCRx 时复位,
当 TAR 的值等于 TACCR0 时置位。
到底是个什么时序呢?
谢谢楼上回答
不过手册上就是这样写的:
输出模式 7 PWM 复位/置位模式:
输出电平在 TAR 的值等于 TACCRx 时复位,
当 TAR 的值等于 TACCR0 时置位。
既然有点不一样就像您写的:1、上升模式:TACCRx >= TACCR0+1
为什么不稍微详细说明白一点呢?
比较值大于周期值,让比较一直不能发生,达到周期值TACCR0之后会一直保持高电平,这是可靠的100%占空比产生方法
若是TACCRx = TACCR0,我不能保证是先复位还是先置位,需要做实验核实下。
还是迷惑
HARDY ZHOU说:
比较值大于周期值,让比较一直不能发生,达到周期值TACCR0之后会一直保持高电平,这是可靠的100%占空比产生方法
若是TACCRx = TACCR0,我不能保证是先复位还是先置位,需要做实验核实下。
既然TACCRx = TACCR0不一定保险,那么在官网的一个文档:PWM DC Motor Control Using Timer A of the MSP430
中,好像TACCRx可以等于0或者等于TACCR0,并没有到TACCR0+1呀
文档中代码如下:
#include "msp430x11x1.h" ; Standard Equations
NAME DCmotorspeedcontroller
;******************************************************************************
;
; Murugavel Raju
; Texas Instruments, Inc
;
;******************************************************************************
;CPU registers used
;******************************************************************************
#define Duty_cycle R6
;******************************************************************************
;Constants
;******************************************************************************
PWM_OUT equ 004h ; bit2 of Port1 / TA1
Period equ 0ffh ; Counts for D/A, 8bits = 256
;******************************************************************************
;
;******************************************************************************
RSEG CSTACK
DS 0
;******************************************************************************
RSEG CODE
;******************************************************************************
RESET mov #SFE(CSTACK),SP ; define stackpointer
call #Init_Sys ; Initialize
Mainloop bit.b #BIT0,&P2IN ; check if 'decrease' button pressed
jz Next1
bit.b #BIT1,&P2IN ; check if 'increase' button pressed
jz Next2
jmp Mainloop ; loop if no button pressed
Next1 cmp #0,Duty_cycle ; check if PWM = 0
jz Mainloop ; repeat loop
dec Duty_cycle ; increment the PWM by one step
jmp SendPWM
Next2 cmp #0ffh,Duty_cycle ; check if 256 steps are done
jz Mainloop ; Repeat for next cycle
inc Duty_cycle ; increment the PWM by one step
SendPWM mov Duty_cycle,&CCR1 ; Send value to PWM output
call #Delay ; insert a small delay between key polling
jmp Mainloop ; repeat loop
;******************************************************************************
Init_Sys; Modules and Controls Registers set-up subroutine
;******************************************************************************
StopWDT mov #WDTPW+WDTHOLD,&WDTCTL ; Stop Watchdog Timer
SetupBC mov.b #XTOFF+RSEL2+RSEL1+RSEL0,&BCSCTL1
; RSEL=7
mov.b #0ffh,&DCOCTL ; DCO selected for highest freq.
SetupP1 mov.b #0,&P1OUT ; P1OUT reset
bis.b #PWM_OUT,&P1SEL ; P1.2/TA1 for PWM OUT
bis.b #0ffh,P1DIR ; P1.2 output for PWM OUT and remaining unused
SetupP2 mov.b #03ch,&P2DIR ; P2.0,P2.1 as inputs,P2.2 to P2.5 outputs(unused)
mov #Period,&CCR0 ; Set Period length for PWM output
mov #0,&CCR1 ; Initial PWM value for output
mov #OUTMOD_7,&CCTL1 ; Set output mode 7 for TA1
SetupTA mov #TASSEL1+MC0,&TACTL ; Set TimerA Up mode, SMCLK as TACLK
mov #0,Duty_cycle ; reset Duty_cycle buffer
ret ; Return from subroutine
;******************************************************************************
Delay; Software delay
;******************************************************************************
push #03FFFh ; Delay to TOS
L1 dec 0(SP) ; Decrement TOS
jnz L1 ; Delay over?
incd SP ; Clean TOS
ret ; Return from subroutine
;******************************************************************************
COMMON INTVEC ; MSP430F1xx Interrupt vectors
;******************************************************************************
ORG RESET_VECTOR
RESET_VEC DW RESET ; POR, ext. Reset, Watchdog
END
虽然我很懒也没精力,要忙忙这个又要忙忙那个,还是想着什么时候写两句验证一下的,尽管要把lauchpad上原有的东西拔下来。
不过我看了这个帖子:PWM -- what is special about 0% and 100% duty-cycle? 后又懒得弄了,弄了也可能和那个帖子的人一样呀。
哪位给解释解释呀