This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994: 5994

Part Number: MSP430FR5994


使用官方的库函数transform_ex1_fft_fixed_q15,在MSP430FR5994上运行时间为57mS,为什么时间这么长?

  • 你好,你的期望值是多少,或者说该运行时间不符合某个手册上的描述吗(如果是的话,请指出具体位置)

  • 您好,我找到时间原因了 ,发现程序运行第二行FFT程序只花了大约4mS,如果运行第三行则需要约57mS,请问这个msp_benchmarkStart和msp_benchmarkStop基准测试是干嘛的?是必须的吗?除此之外,我还有一些问题

    使用5994板卡上面的ADC12_B采数,差模输入,量化结果为12位,左对齐,带符号,用定时器TA0.3触发,PWM频率是32kHz,一组数256个,这样的数应该如何转化成transform_ex1_fft_fixed_q15案例中的FFT输入信号input?input是什么类型的数值?

  • 请问这个msp_benchmarkStart和msp_benchmarkStop基准测试是干嘛的

    从资料上来看就是计数用的。

    使用5994板卡上面的ADC12_B采数,差模输入,量化结果为12位,左对齐,带符号,用定时器TA0.3触发,PWM频率是32kHz,一组数256个,这样的数应该如何转化成transform_ex1_fft_fixed_q15案例中的FFT输入信号input?input是什么类型的数值?

    可以看下下面的资料:

    software-dl.ti.com/.../transform_ex1_fft_fixed_q15_8c-example.html