This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: 不同材质的管道中液体流量的测量问题

Part Number: MSP430FR6047

你好,目前我在进行流量计对不同材质管道的适应性检测,所采用的换能器安装方式为“V”型安装,如下图所示:

当装置安装在PVC管道上时,在上位机软件上貌似可以看到两个特征明显的波瓣,当Gap between pulse start and ADC capture 此参数为40时,波形图如下:

Gap between pulse start and ADC capture 此参数为80时,波形图如下:

当Gap between pulse start and ADC capture 此参数为60时,可以很清楚的看到两个波瓣的分界情况:

但是,只有当Gap between pulse start and ADC capture 此参数为80时,所显示的波瓣才可以正确的进行流量计算,也就是第二个波瓣才可以进行流量计算,第一个波瓣的信号强度貌似较低,上位机会报错,无法进行计算。

我现在的问题是,当我把测量装置放到不锈钢管道上时,上位机所看到的波瓣只有一个,当Gap between pulse start and ADC capture 此参数为40时,波形为

此波形无法进行流量计算,会频繁的报错,但是当Gap between pulse start and ADC capture 此参数为80时,并没有和PVC管道一样出现第二个波瓣,而是一堆杂乱信号,如下图所示

因此该装置无法在不锈钢管道上进行流量测量,所以我想请教一下,出现这种问题的原因可能是什么,我要采取怎么样的解决方法。如有解答,不胜感激。

附上上位机配置