This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A的RAM使用问题超过data超过4K



你好,请教个问题。

我 的程序比较大,需要开辟大的数组作为缓存区域来存放数据,仿真运行时会出现stack溢出,我调整了IAR中stack的大小,使之初步满足自定义的数组的大小。

现在的问题现象是,当定义一个长度为512的数组,使用JTAG监测到数组的地址位于16KRAM的第一个Sec(2998H~2B97H,第一个4KRAM)。但是增加一个大小为512的数组时,编译能通过,但是程序不能运行,然后定义个小点的数组(地址小于2BFFH),可以正常运行。

需要解决的问题汇总:

1、程序中还需要定义几个大数组作为全局变量,怎么把3C00H~4BFFH的RAM区域使用起来?stack还需要怎么调整?

2、是不是定义的数组局部变量,存放在stack中,栈顶地址为5BFFH,分配是按照从栈顶到栈底的原则进行分配?

3、heap在什么情况下需要调整IAR中默认的160字节的大小?

急需解决,谢谢!