This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: MSP430F5529的SPI屏蔽了按键中断问题

Part Number: MSP430F5529


MSP430F5529硬件spi方式驱动一个spi的液晶,可以正常显示,但是按键却无法进入中断,我的相同程序在msp430f2553中是正常的,这是什么原因造成的?

经过排查问题,用模拟spi方式驱动就没有任何问题,我想知道根本的原因。

void initSPI()
{
    //SPI Pins
    P3SEL |= BIT3 + BIT4;                     // P3.3,4 option select
    P2SEL |= BIT7;                            // P2.7 option select

    //Clock Polarity: The inactive state is high
    //MSB First, 8-bit, Master, 3-pin mode, Synchronous
    UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
    UCA0CTL0 |= UCMST+UCSYNC+UCCKPL+UCMSB;    // 3-pin, 8-bit SPI master
                                                // Clock polarity high, MSB
    UCA0CTL1 |= UCSSEL_2;                     // SMCLK
    UCA0BR0 |= 0x02;                          // /2
    UCA0BR1 = 0;                              //
    UCA0MCTL = 0;                             // No modulation
    UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
    UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt

    P1OUT &= ~BIT2;                           // Now with SPI signals initialized,
    __delay_cycles(100000);
    P1OUT |= BIT2;                            // reset slave
    __delay_cycles(100000);                   // Wait for slave to initialize
}

void SPI_WriteByte(uint8_t MST_Data)
{  
    UCA0TXBUF = MST_Data;                     // Transmit first character
    while (!(UCA0IFG & UCTXIFG));             // USCI_A0 TX buffer ready?
                                              // guochl:上面这句没有不行,放在传输之前也不行,不知道?
}